This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:eval-ad7944_85_86edz [09 Mar 2012 19:13] – c Catherine Redmond | resources:eval:eval-ad7944_85_86edz [26 Sep 2013 22:30] – [Jumpers, Solder Pads and test points] Alan Walshe | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== | + | ====== |
===== Features ===== | ===== Features ===== | ||
* **Full-featured evaluation board for the [[adi> | * **Full-featured evaluation board for the [[adi> | ||
- | * **PC Control in conjunction with the converter and evalaution | + | * **PC Control in conjunction with the converter and evaluation |
* **PC software for control and data analysis of time and frequency domain** | * **PC software for control and data analysis of time and frequency domain** | ||
* **Versatile analog signal conditioning circuitry** | * **Versatile analog signal conditioning circuitry** | ||
Line 8: | Line 8: | ||
* **Standalone capability** | * **Standalone capability** | ||
{{ : | {{ : | ||
+ | |||
==== System Requirements ==== | ==== System Requirements ==== | ||
Line 39: | Line 40: | ||
======General Description====== | ======General Description====== | ||
- | The EVAL-AD79XXEDZ is an evaluation board for the 20-lead [[adi> | + | The EVAL-AD79XXEDZ is an evaluation board for the 20-lead [[adi> |
- | On-board components include a high precision, buffered band gap 5.0 V reference ([[adi> | + | On-board components include a high precision, buffered band gap 5.0 V reference ([[adi> |
The evaluation board interfaces to the CED capture board by using a 96-pin DIN connector. In addition, SMB connectors, J1 and J2, are provided for the low noise analog signal source. | The evaluation board interfaces to the CED capture board by using a 96-pin DIN connector. In addition, SMB connectors, J1 and J2, are provided for the low noise analog signal source. | ||
- | ===== Quickstart ===== | + | ====== Quickstart |
- Install the software from the enclosed CD or by downloading from the Analog Devices, Inc., Website, at www.analog.com. | - Install the software from the enclosed CD or by downloading from the Analog Devices, Inc., Website, at www.analog.com. | ||
- Ensure the evaluation board is disconnected from the USB port of the PC while installing the software. | - Ensure the evaluation board is disconnected from the USB port of the PC while installing the software. | ||
Line 52: | Line 53: | ||
- Connect the EVAL-CED1Z board to the PC via the USB cable. | - Connect the EVAL-CED1Z board to the PC via the USB cable. | ||
- Choose to automatically search for the drivers for the [[adi> | - Choose to automatically search for the drivers for the [[adi> | ||
- | - For Windows | + | - For Windows® |
- | - Launch the EVAL-AD7944/ | + | - Launch the EVAL-AD7944/ |
- | - Select the appropriate device from the drop down menu [[adi> | + | - Select the appropriate device from the drop-down menu [[adi> |
- Apply a signal source to the AIN+/AIN− SMB inputs on the evaluation board. | - Apply a signal source to the AIN+/AIN− SMB inputs on the evaluation board. | ||
- Configure the signal source for the appropriate signal applied to the input of the device. | - Configure the signal source for the appropriate signal applied to the input of the device. | ||
- | - Capture data by initiating a single capture (F3) or a continuous capture (F4). | + | - Capture data by initiating a single capture |
- See details on configuring the software in the Running the ADC Analysis Software section. | - See details on configuring the software in the Running the ADC Analysis Software section. | ||
Note that the measurements made by Analog Devices use the Audio Precision SYS-2522. | Note that the measurements made by Analog Devices use the Audio Precision SYS-2522. | ||
{{ : | {{ : | ||
+ | **//Figure 2. Hardware Configuration—Setting up the Evaluation Board//** | ||
====== Evaluation Board Hardware ====== | ====== Evaluation Board Hardware ====== | ||
- | The low power, [[adi> | + | |
- | The evaluation board is designed to demonstrate the performance of the ADC and to provide an easy-to-understand interface for a variety of system applications. | + | The low power, [[adi> |
- | The evaluation board is ideal for use with the Analog Devices Converter and Evaluation Development EVAL-CED1Z (CED). The design offers the flexibility of applying external control signals and is capable of generating conversion results on parallel 16-bit wide buffered outputs. | + | |
- | The figure above shows the EVAL-AD7944/ | + | The evaluation board is designed to demonstrate the performance of the ADC and to provide an easy-to-understand interface for a variety of system applications. |
- | This evaluation board is a 6-layer board carefully laid out and tested to demonstrate the specific high accuracy performance of the [[adi> | + | |
+ | The evaluation board is ideal for use with the Analog Devices Converter and Evaluation Development EVAL-CED1Z (CED). The design offers the flexibility of applying external control signals and is capable of generating conversion results on parallel 16-bit wide buffered outputs.\\ | ||
+ | |||
+ | Figure 2 shows the EVAL-AD7944/ | ||
+ | |||
+ | This evaluation board is a 6-layer board carefully laid out and tested to demonstrate the specific high accuracy performance of the [[adi> | ||
===== Device Description ===== | ===== Device Description ===== | ||
- | The [[adi> | + | The [[adi> |
- | These ADCs are low power and high speed and include an internal conversion clock, an internal reference (and buffer), error correction circuits, and a versatile serial interface port. On the rising edge of CNV, the ADC samples an analog input, IN+, between 0 V and REF with respect to the ground sense, IN−. The ADCs feature a very high sampling rate turbo mode (TURBO is high) and a reduced power normal mode (TURBO is low) for low power applications where the power is scaled with the throughput. A full description of these products is available in their respective data sheets and should be consulted when using this evaluation board. | + | |
+ | These ADCs are low power and high speed and include an internal conversion clock, an internal reference (and buffer), error correction circuits, and a versatile serial interface port. On the rising edge of CNV, the ADC samples an analog input, IN+, between 0 V and REF with respect to the ground sense, IN−. The ADCs feature a very high sampling rate turbo mode (TURBO is high) and a reduced power normal mode (TURBO is low) for low power applications where the power is scaled with the throughput. A full description of these products is available in their respective data sheets and should be consulted when using this evaluation board.\\ | ||
===== Power Supplies ===== | ===== Power Supplies ===== | ||
- | Power is supplied to the board through | + | Power is supplied to the board through |
- | Standalone Operation | + | |
- | The evaluation board can be used in standalone mode without the CED controller board. In this case, power supplies need to be applied to the board at P4 or at the relevant test points. At a minimum, the board requires ±5 V, +12 V, +7 V, or + 2.5 V. See Figure 23 for details regarding power supply connections. | + | ===== Standalone Operation |
- | ==== Grounding ==== | + | The evaluation board can be used in standalone mode without the CED controller board. In this case, power supplies need to be applied to the board at P4 or at the relevant test points. At a minimum, the board requires ±5 V, +12 V, +7 V, or + 2.5 V. See the Design Support Package section |
+ | |||
+ | ===== Grounding | ||
The evaluation board ground plane is separated into two sections: a plane for the digital interface circuitry and an analog plane for the analog input and external reference circuitry. To attain high resolution performance, | The evaluation board ground plane is separated into two sections: a plane for the digital interface circuitry and an analog plane for the analog input and external reference circuitry. To attain high resolution performance, | ||
- | ==== Conversion Control ==== | + | ===== Conversion Control |
- | The on-board FPGA performs a number of digital functions, one of them being the deserialization of the serial conversion results as the CED data capture | + | The on-board FPGA performs a number of digital functions, one of them being the deserialization of the serial conversion results as the CED data capture |
+ | |||
+ | ===== Analog Inputs===== | ||
+ | The analog inputs to the evaluation board are J1, J2, and SMB (push on). These inputs are buffered with dedicated amplifier circuitry (A2, A3, and discretes) to allow configuration changes such as positive or negative gain, input range scaling, filtering, addition of a dc component, and use of different op amps and supplies. The analog input amplifiers are set as unity-gain buffers at the factory. The supplies are selectable with solder pads and are set for the +7 V to −5 V ranges.\\ | ||
+ | |||
+ | The default configuration sets both A2 and A3 at midscale generated from either a buffered reference voltage divider or the internal reference of the ADC. \\ | ||
+ | |||
+ | The evaluation board is factory configured for providing either a single-ended path or a fully differential path. Because the AD7986 is differential, | ||
+ | |||
+ | For dynamic performance, | ||
- | ==== Analog Inputs==== | ||
- | The analog inputs to the evaluation board are J1, J2, and SMB (push on). These inputs are buffered with dedicated amplifier circuitry (A2, A3, and discretes) to allow configuration changes such as positive or negative gain, input range scaling, filtering, addition of a dc component, and use of different op-amps and supplies. The analog input amplifiers are set as unity-gain buffers at the factory. The supplies are selectable with solder pads and are set for the +7 V to −5 V ranges. | ||
- | The default configuration sets both A2 and A3 at midscale generated from either a buffered reference voltage divider or the internal reference of the ADC. | ||
- | The evaluation board is factory configured for providing either a single-ended path or a fully differential path. Because the AD7986 is differential, | ||
- | For dynamic performance, | ||
Because the evaluation board uses the amplifiers in unity gain, the noninverting input has a common-mode input with a 590 Ω series resistor, which needs to be taken into account when directly connecting a source (voltage divider). | Because the evaluation board uses the amplifiers in unity gain, the noninverting input has a common-mode input with a 590 Ω series resistor, which needs to be taken into account when directly connecting a source (voltage divider). | ||
- | ==== Serial Interface ==== | + | ===== Serial Interface |
The 3-wire serial interface SDI, SCK, and SDO together with CNV are present on the digital interface test points, and FPGA buffered versions are on the 96-pin connector, P1. The on-board Altera FPGA can be reprogrammed to the user’s configuration as the serial device and U1 is in-circuit programmable. | The 3-wire serial interface SDI, SCK, and SDO together with CNV are present on the digital interface test points, and FPGA buffered versions are on the 96-pin connector, P1. The on-board Altera FPGA can be reprogrammed to the user’s configuration as the serial device and U1 is in-circuit programmable. | ||
- | ==== Jumpers, Solder Pads and test points ==== | + | ===== Jumpers, Solder Pads and test points |
A number of 3-pin jumpers, solder pads, and test points are provided on the evaluation board and are detailed in Table 1, Table 2, and Table 7. Most of the 3-pin jumpers are used for the reference selection of the ADCs (see the Reference Options section for details and settings). | A number of 3-pin jumpers, solder pads, and test points are provided on the evaluation board and are detailed in Table 1, Table 2, and Table 7. Most of the 3-pin jumpers are used for the reference selection of the ADCs (see the Reference Options section for details and settings). | ||
- | === Table 1. 3-Pin Jumper Descriptions | + | == Table 1. 3-Pin Jumper Descriptions == |
^Jumper ^ Default Position ^ Function ^ | ^Jumper ^ Default Position ^ Function ^ | ||
|P2 | REF to middle | ADC REF/REFIN select| | |P2 | REF to middle | ADC REF/REFIN select| | ||
Line 105: | Line 119: | ||
|P12 | PDREF to VIO | Selection of either the internal reference of the ADC or an external reference. | | |P12 | PDREF to VIO | Selection of either the internal reference of the ADC or an external reference. | | ||
- | === Table 2. Solder Pad Descriptions | + | == Table 2. Solder Pad Descriptions == |
^Solder Pad ^ Default Position ^ Function ^ | ^Solder Pad ^ Default Position ^ Function ^ | ||
| JP1, JP2 | A2, A3 (bottom to middle)|ADC inputs: bottom pad to middle pad are for A2/A3 output. To bypass and use J1/J2 directly, solder top pad to middle pad.| | | JP1, JP2 | A2, A3 (bottom to middle)|ADC inputs: bottom pad to middle pad are for A2/A3 output. To bypass and use J1/J2 directly, solder top pad to middle pad.| | ||
Line 116: | Line 130: | ||
|DVDD |+2.5 V |ADC DVDD (digital core) supply: selection of 2.5 V or 5 V on the board or externally. To prevent permanent damage to the ADC, do not solder to 5 V or connect this supply to > 2.5 V.| | |DVDD |+2.5 V |ADC DVDD (digital core) supply: selection of 2.5 V or 5 V on the board or externally. To prevent permanent damage to the ADC, do not solder to 5 V or connect this supply to > 2.5 V.| | ||
|BVDD |+5 V |ADC BVDD 5 V supply: selection of 5 V on the board or externally. For an external reference, the best performance is obtained when the reference source that is connected to the REF pins and BVDD are the same. See the External Reference: Factory Configuration section for details.| | |BVDD |+5 V |ADC BVDD 5 V supply: selection of 5 V on the board or externally. For an external reference, the best performance is obtained when the reference source that is connected to the REF pins and BVDD are the same. See the External Reference: Factory Configuration section for details.| | ||
- | |VIO |+2.5 V |ADC digital input/ | + | |VIO |+2.5 V |ADC digital input/ |
Solder pads are factory configured for the device being evaluated. | Solder pads are factory configured for the device being evaluated. | ||
- | ==== Reference Options ==== | + | ===== Reference Options |
- | The AD7944/ | + | The AD7944/ |
- | === External Reference: Factory Configuration === | + | |
- | The evaluation board includes the ADR435 which is a 5 V precision voltage reference. This reference can drive the ADCs and the REF pin directly or it can be buffered with the AD8032; both of which serve as the factory default setting. The best attainable SNR is achieved by using the maximum reference voltage of 5 V (see the appropriate ADC datasheet for details). | + | ==== External Reference: Factory Configuration |
- | === Table 3. Factory Reference Jumper Configuration | + | The evaluation board includes the [[adi>ADR435]] which is a 5 V precision voltage reference. This reference can drive the ADCs and the REF pin directly or it can be buffered with the [[adi>AD8032]]; both of which serve as the factory default setting. The best attainable SNR is achieved by using the maximum reference voltage of 5 V (see the appropriate ADC datasheet for details). |
+ | |||
+ | == Table 3. Factory Reference Jumper Configuration == | ||
^Jumper ^Setting ^ | ^Jumper ^Setting ^ | ||
|P2 |REF and middle| | |P2 |REF and middle| | ||
Line 131: | Line 147: | ||
|P11 |REFIN to GND| | |P11 |REFIN to GND| | ||
|P12 |PDREF to VIO| | |P12 |PDREF to VIO| | ||
- | |BVDD |5 V (factory)| | + | |BVDD |5 V (factory |
To use an external reference source as opposed to the internal reference, there are two methods available, as follows: | To use an external reference source as opposed to the internal reference, there are two methods available, as follows: | ||
Line 138: | Line 154: | ||
==== ADC Reference Supply, BVDD ==== | ==== ADC Reference Supply, BVDD ==== | ||
- | The evaluation board includes a 5 V source for the ADC reference supply, BVDD, set with a pair of solder pads of either 5 V or EXT_B, and a test point, EXT_B {so BVDD can be set with EXT_B as the solder pad and EXT_B as the test point as well?}. For the best performance, | + | The evaluation board includes a 5 V source for the ADC reference supply, BVDD, set with a pair of solder pads of either 5 V or EXT_B, and a test point, EXT_B. For the best performance, |
==== Internal 4.096 V Reference ==== | ==== Internal 4.096 V Reference ==== | ||
- | The ADC has an internal 4.096 V precision reference and can be used on most applications. Connecting PDREF to GND enables the internal reference. When the internal reference is enabled, 4.096 V as well as a 1.2 V band gap are present on the ADC REF pin and test point. Note that external sources must not be connected to these test points because they {what are “they”? The external sources | + | The ADC has an internal 4.096 V precision reference and can be used on most applications. Connecting PDREF to GND enables the internal reference. When the internal reference is enabled, 4.096 V as well as a 1.2 V band gap are present on the ADC REF pin and test point. Note when using the internal reference, |
+ | |||
+ | == Table 4. Internal Reference Jumper Configuration == | ||
+ | ^Jumper ^Setting^ | ||
+ | |P2 |Open| | ||
+ | |P9 |REFS to VREF| | ||
+ | |P10 |Don’t care| | ||
+ | |P11 |Open| | ||
+ | |P12 |PDREF to GND| | ||
+ | |BVDD |5 V (factory)| | ||
+ | |||
+ | ==== Internal Reference Buffer ==== | ||
+ | The internal reference buffer is useful when using an external 1.2 V reference. When using the internal reference buffer, applying 1.2 V to REFIN, which is directly connected to the REFIN pin of the ADC, produces 4.096 V at the REF pin of the ADC. | ||
+ | Because there is no 1.2 V reference on the board, there are two methods to generate a 1.2 V reference. The first method is to connect an external source to the REFIN test point using the jumper settings listed in Table 5. | ||
+ | |||
+ | == Table 5. Fully External Reference Buffer Jumper Configuration: | ||
+ | ^Jumper ^Setting^ | ||
+ | |P2 |Open| | ||
+ | |P9 |Don’t care| | ||
+ | |P10 |Don’t care| | ||
+ | |P11 |Open| | ||
+ | |P12 |PDREF to VIO| | ||
+ | |BVDD |5 V (factory default)| | ||
+ | |||
+ | The second method is to use the U2 op amp to voltage divide down the 5 V output of the [[adi> | ||
+ | == Table 6. Fully External Reference Buffer Jumper Configuration: | ||
+ | |||
+ | ^Jumper ^Setting^ | ||
+ | |P2 |REFIN to middle| | ||
+ | |P9 |REFS to VREF| | ||
+ | |P10 |BUF to middle| | ||
+ | |P11 |REFIN to Pin 1| | ||
+ | |P12 |PDREF to VIO| | ||
+ | |BVDD |5 V (factory default)| | ||
+ | |||
+ | |||
+ | ====== Evaluation Board Software ====== | ||
+ | |||
+ | ===== Important Software Pre-Installation Information ===== | ||
+ | The [[adi> | ||
+ | |||
+ | ==== Software Installation ==== | ||
+ | It is recommended to close all Windows® applications prior to installing the software. | ||
+ | The evaluation board comes with a CD as part of the evaluation kit. The latest software versions are always available from the Analog Devices product page, visit [[www.analog.com]]. Note that the user must accept the license agreement during the installation process.\\ | ||
+ | |||
+ | {{ : | ||
+ | **//Figure 3. To Install, the User Must Accept License Agreement// | ||
+ | |||
+ | After downloading the software, it is recommended to use the WinZip extract function to extract all of the necessary components rather than immediately selecting **setup.exe** from within the zipped file. | ||
+ | After extracting the software, click **setup.exe** in the folder created during the extraction process and follow the instructions on the screen. \\ | ||
+ | |||
+ | If another version of the software already exists on the computer, it may be necessary to remove it. To remove prior versions of the software, click the Windows **Start** button, select **Control Panel**, and then select **Add or Remove Programs**. When the list populates, navigate to **Analog Devices High Resolution sampling ADC’s Evaluation Software** or **PulSAR Evaluation Software** and select **Remove**. \\ | ||
+ | |||
+ | === Typical Install Process === | ||
+ | |||
+ | {{ : | ||
+ | **//Figure 4. Initiating Install from setup.exe// | ||
+ | |||
+ | {{ : | ||
+ | **//Figure 5. Default Location for Install Files//** | ||
+ | |||
+ | {{ : | ||
+ | **//Figure 6. Installing Software// | ||
+ | |||
+ | {{ : | ||
+ | **//Figure 7. Install Complete// | ||
+ | |||
+ | ==== USB Drivers ==== | ||
+ | The software also installs the necessary USB drivers through a separate installation process. When the software installation completes the drivers installation wizard displays: click **Install** to install the drivers automatically, | ||
+ | |||
+ | {{ : | ||
+ | **//Figure 8. Driver Install Process// | ||
+ | |||
+ | {{ : | ||
+ | **//Figure 9. Install Complete// | ||
+ | |||
+ | After installing the software and drivers, power the CED board and connect it to the PC USB 2.0 port, at which time the **Welcome to the Found New Hardware Wizard** initiates. | ||
+ | {{ : | ||
+ | **//Figure 10. Found New Hardware// | ||
+ | |||
+ | When installed properly, the hardware wizard displays the following message, shown in Figure 11, signaling that the evaluation board software is setup and ready to use. | ||
+ | {{ : | ||
+ | **//Figure 11. Evaluation Board Software Installation Complete// | ||
+ | |||
+ | On some PCs, the **Found New hardware Wizard** may show up again and, if so, follow the same procedure to install it properly. Use the **Device Manager**, shown in Figure 12, to verify that the driver was installed correctly. | ||
+ | {{ : | ||
+ | **//Figure 12. Device Manager Verification// | ||
+ | |||
+ | === Troubleshooting the Installation === | ||
+ | |||
+ | If the driver was not installed properly, Windows does not recognize the CEDIZ board and the Device Manager menu displays a question mark for **Other devices**. | ||
+ | {{ : | ||
+ | **//Figure 13. Device Manager Menu Displaying Unrecognized Device// | ||
+ | |||
+ | The USB device can be opened to view its uninstalled properties, as shown in Figure 14. | ||
+ | {{ : | ||
+ | //**Figure 14. USB Device Uninstalled Properties**// | ||
+ | |||
+ | The most usual reason for uninstalled properties is caused by the installation of the software and drivers by a user without administrative privileges. If this is the case, log on as an administrator with full privileges and reinstall the software. | ||
+ | |||
+ | |||
+ | ==== Running the Evaluation Software ==== | ||
+ | |||
+ | The evaluation board includes software for analyzing the AD7944, AD7985, and AD7986. The [[adi> | ||
+ | |||
+ | * Histogram for determining code transition noise (dc).\\ | ||
+ | * Fast Fourier transforms (FFT) for signal-to-noise ratio (SNR), SNR and signal-to-noise-and-distortion (SINAD), total harmonic distortion (THD), and spurious free dynamic range (SFDR).\\ | ||
+ | * Decimation (digital filtering).\\ | ||
+ | * | ||
+ | The software is located at < | ||
+ | To run the software, select the program from either location. | ||
+ | |||
+ | ==== Running the ADC Analysis Software ==== | ||
+ | The evaluation board includes software for analyzing the [[adi> | ||
+ | |||
+ | * Histogram for determining code transition noise (dc). | ||
+ | * FFT for SNR, SNR and SINAD, THD, and SFDR.\\ | ||
+ | * | ||
+ | Refer to Figure 15 to Figure 20 for additional details and features of the software.\\ | ||
+ | |||
+ | The ADC analysis software is located at C:\Program Files\Analog Devices\ PulSAR ADC Evaluation Software\Eval PulSAR CED.exe. A shortcut is also added to the Windows **Start** menu under **Analog Devices PulSAR ADC Evaluation Software, Eval PulSAR CED.** To run the software, select the program from either location. | ||
+ | |||
+ | ===== Software Operation ===== | ||
+ | The following steps detail the operation of the software located in the default directory: | ||
+ | < | ||
+ | |||
+ | {{ : | ||
+ | //**Figure 15. Setup Screen**// | ||
+ | |||
+ | - To start the software, click the arrow in the upper left corner of the screen. When running, the arrow icon is displayed as shown in the area in Figure 15 marked with the Number 1. | ||
+ | - Select the device to be evaluated (see the area in Figure 15 marked with the Number 2). | ||
+ | - Set the controls (see the area in Figure 15 marked with the Number 3) for the following: | ||
+ | - **Sample Frequency: | ||
+ | - **Input Range:** Because the ADCs have a variable input range depending on the reference voltage, select the correct one (4.096 V or 5 V) to display the correct LSB size. | ||
+ | - **Interface Mode:** Options for using or not using the busy mode. In busy mode, the SDO can be monitored to see the actual conversion time (BUSY high to low transition). | ||
+ | - **Turbo CTRL:** Select the fastest mode, turbo mode, or normal mode. Note that the throughput must be manually changed when changing modes. | ||
+ | - **CNV Mode:** Selects between continuous (Cont.) or burst conversion modes. In continuous mode, the ADC is continuously converting. In burst mode, the ADC does not continuously convert. | ||
+ | - **Coding:** For the AD7986, **2 compl** must be selected in the **Coding** field because the ADC result is always twos complement. For the AD7985 and AD7944, binary is set because the ADC output is straight binary. | ||
+ | - Use the controls shown in the area of Figure 15 marked with the Number 4 for functions such saving, printing, help, and so forth. These functions | ||
+ | - **Save (F5):** In the **Save** **(F5)** pull-down menu, there are several options as follows: | ||
+ | - **LV Config:** selects the LabVIEW® configuration, | ||
+ | - **Html:** saves the current screen shot to an html file. | ||
+ | - **Spreadsheet: | ||
+ | - **Stop (F10):** Click **Stop (F10)** to stop running the software. Likewise, clicking the stop sign icon, on the top menu bar also stops the software. | ||
+ | - **RESET:** click **RESET** to reset the CED capture board. | ||
+ | |||
+ | ===== Context Help ===== | ||
+ | ==== On-Screen Help ==== | ||
+ | To use the on-screen help. Select **Help**, **Show Context Help** or click **Help (F1)**. These function areas on the screen are indicated by Number 1 in Figure 16. Hovering the cursor over most screen items displays useful information for the particular control or displayed unit.\\ | ||
+ | |||
+ | {{ : | ||
+ | **//Figure 16. Context Help and Histogram Controls// | ||
+ | |||
+ | === Histogram Controls === | ||
+ | The histogram controls, shown in the area indicated by Number 2 in Figure 16, are used for axes and zooming panning, as follows: | ||
+ | |||
+ | == Graph Axis Lock == | ||
+ | Locks the graph axis to automatically fit the data.\\ | ||
+ | |||
+ | == Axis Rescaling == | ||
+ | Uses the last axis set by the user. These allow the user to rescale the x- and y-axis, respectively, | ||
+ | |||
+ | == Axis Properties == | ||
+ | These are used to set the x- and y-axis properties, such as format, precision, color, and so forth.\\ | ||
+ | |||
+ | == Cursor Display == | ||
+ | Displays the cursor.\\ | ||
+ | |||
+ | == Zooming == | ||
+ | Zooms in and out.\\ | ||
+ | |||
+ | == Panning == | ||
+ | Use to pan.\\ | ||
+ | |||
+ | == Graph Properties == | ||
+ | Sets various graph properties such as graph type, colors, lines, and so forth. | ||
+ | |||
+ | ==== Histogram and Oscilloscope Charts ==== | ||
+ | |||
+ | The areas of the **Raw Data Capture** window that pertain to working with histogram | ||
+ | |||
+ | {{ : | ||
+ | **//Figure 17. Histogram Data Window// | ||
+ | |||
+ | ==== Single or Continuous Capture ==== | ||
+ | |||
+ | Use the buttons shown in Section 1 in Figure 17 to perform either a single capture or continuous capture of data. Enter the number of samples that are required in the **# of Samples (k)** field (located to the left of the **Single Capture (F3)** button). The statistics for the x- and y-axes are displayed in the **Histogram Data** section of the window, shown as the Number 2 and Number 3 areas within Figure 17.\\ | ||
+ | |||
+ | The graphic results are displayed in the chart area of the window. Note that the results can be displayed as either a histogram (see Figure 18) or an oscilloscope (see Figure 19) by selecting the relevant tab, **Oscilloscope**, | ||
+ | |||
+ | Time domain data can also be viewed by using the **Oscilloscope** tab. In addition, the charts can be displayed together when the **Summary** tab is selected (see Figure 21).\\ | ||
+ | |||
+ | {{ : | ||
+ | **//Figure 18. Histogram Chart Display// | ||
+ | |||
+ | |||
+ | {{ : | ||
+ | //**Figure 19. Oscilloscope Chart Display (Time Domain)**// | ||
+ | |||
+ | {{ : | ||
+ | **//Figure 20. Oscilloscope// | ||
+ | |||
+ | {{ : | ||
+ | //**Figure 21. Summary Tab**//\\ | ||
+ | |||
+ | |||
+ | == FFT Spectrum Data == | ||
+ | To review the FFT spectrum data, select the **Spectrum** tab in the **Raw Data Capture** window. Figure 22 shows the FFT spectrum window and sections numbered 1, 2, and 3 of this window are described as follows: | ||
+ | |||
+ | == Displaying the FFT == | ||
+ | |||
+ | From the **Raw Data Capture** window, in the section of Figure 22 labeled with Number 1, select the **Spectrum** tab to display the FFT when the spectrum chart is selected.\\ | ||
+ | |||
+ | == Displaying the Spectrum Data == | ||
+ | |||
+ | The **Spectrum Data** section (Number 2 and Number 3 in Figure 22), is located beneath the spectrum chart. These areas of the **Spectrum Data** section display the data for the x-axis (shown in the area labeled as Number 2) and y-axis, (shown in the area labeled as Number 3).\\ | ||
+ | |||
+ | {{ : | ||
+ | **//Figure 22. FFT Spectrum// | ||
+ | \\ | ||
+ | ====== Troubleshooting ====== | ||
+ | |||
+ | ===== Software Tips ===== | ||
+ | |||
+ | * Always install the software from the CD or the Analog Devices website prior to connecting hardware to the PC. | ||
+ | * Always allow the installation to fully complete (the software is a two part installation: | ||
+ | * When you first plug in the board via the USB cable, allow the **New Found Hardware Wizard** to run completely. Though this may take some time, it is required prior to starting the software. | ||
+ | * Where the board does not appear to be functioning, | ||
+ | |||
+ | ===== Hardware Tips ===== | ||
+ | |||
+ | If the software does not read any data back, take the following steps: | ||
+ | - Check that power is applied to the CED board and that the voltages are present on the P connectors as described in Table 3. | ||
+ | - Confirm the signal source is applied and outputting the expected signal. | ||
+ | - Probe different points in the signal path to ensure that the applied signal is present at the input of both the driver amplifiers and the ADC. | ||
+ | If there are issues getting SNR performance, | ||
+ | * Some signal sources may require a filter in series to achieve performance. The SNR measurements for this board were tested with the AP-2322 signal source. This is a high performance audio analyzer and source. | ||
+ | * To achieve best SNR performance, | ||
+ | |||
+ | ====== Design Support Package ====== | ||
+ | ===== Schematics ===== | ||
+ | {{: | ||
+ | |||
+ | ===== Gerber Files ===== | ||
+ | {{: | ||
+ | |||
+ | ===== Bill Of Materials ===== | ||
+ | {{: | ||
+ | |||
+ | ===== Software ===== | ||
+ | Software compatible with CED evaluation board available **[[adi> | ||
+ | ====== Related Links ====== | ||
+ | ^Resource ^Description^ | ||
+ | |[[adi> | ||
+ | |[[adi> | ||
+ | |[[adi> | ||
+ | |[[adi> | ||
+ | |[[adi> | ||
+ | |[[adi> | ||
+ | |[[adi> | ||
+ | |[[adi> | ||
+ | |[[adi> | ||
+ | |[[adi> | ||
+ | |[[adi> | ||
+ | |[[adi> |