This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:eval-ad7944_85_86edz [26 Sep 2013 22:30] Alan Walshe [Jumpers, Solder Pads and test points] |
resources:eval:eval-ad7944_85_86edz [06 Apr 2021 10:28] Catherine Redmond [Software Installation] |
||
---|---|---|---|
Line 200: | Line 200: | ||
==== Software Installation ==== | ==== Software Installation ==== | ||
It is recommended to close all Windows® applications prior to installing the software. | It is recommended to close all Windows® applications prior to installing the software. | ||
- | The evaluation board comes with a CD as part of the evaluation kit. The latest software versions are always available from the Analog Devices product page, visit [[www.analog.com]]. Note that the user must accept the license agreement during the installation process.\\ | + | The evaluation board comes with a CD as part of the evaluation kit. The latest software versions are always available from the Analog Devices product page, visit www.analog.com. Note that the user must accept the license agreement during the installation process.\\ |
{{ :resources:eval:10387-003.jpg?300 |}} | {{ :resources:eval:10387-003.jpg?300 |}} |