Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:eval-ad3552r-user-guide [04 Oct 2021 18:01] – User Guide Update_2.0 Toni Almagroresources:eval:eval-ad3552r-user-guide [04 Oct 2021 18:04] (current) – [Installing The Software] Toni Almagro
Line 34: Line 34:
   - Go to Available Packages, select Board.AD35X2R and click on the Install Selected button at the bottom of the list. Once the plugin is installed, it moves to the Installed Packages section.   - Go to Available Packages, select Board.AD35X2R and click on the Install Selected button at the bottom of the list. Once the plugin is installed, it moves to the Installed Packages section.
   - Click on the Home item on the left-hand menu. If the EVALAD3552R board is connected it will show up in the Attached Hardware section as shown in Figure 2. If you don't have an EVAL-AD3552R board, you can still explore the functionality of the plugin by double clicking on the desired board in the Explore Without Hardware list.   - Click on the Home item on the left-hand menu. If the EVALAD3552R board is connected it will show up in the Attached Hardware section as shown in Figure 2. If you don't have an EVAL-AD3552R board, you can still explore the functionality of the plugin by double clicking on the desired board in the Explore Without Hardware list.
-{{:resources:eval:ad3552r-plug-in_manager_with_red_squares.png?nolink&600|}}+{{:resources:eval:ad3552r-plug-in_manager_with_red_squares.png?nolink&400|}}
 \\ \\
 **//Figure 1. Plug-in Manager//** **//Figure 1. Plug-in Manager//**
 \\ \\
-{{:resources:eval:ad3552r-start_tab_with_red_squares.png?nolink&600|}}+{{:resources:eval:ad3552r-start_tab_with_red_squares.png?nolink&400|}}
 \\ \\
 **//Figure 2. Start Tab//** **//Figure 2. Start Tab//**
resources/eval/eval-ad3552r-user-guide.txt · Last modified: 04 Oct 2021 18:04 by Toni Almagro