Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:dpg:eval-ad9739a [21 Sep 2021 10:20]
Melissa Lorenz Lacanlale [Files included in the AD9739A Update:]
resources:eval:dpg:eval-ad9739a [28 Sep 2021 05:11] (current)
Melissa Lorenz Lacanlale Update to SDPH1 and ADSV7
Line 36: Line 36:
   * [[adi>​eval-ad9739a|AD9739A-EBZ]] Evaluation Board   * [[adi>​eval-ad9739a|AD9739A-EBZ]] Evaluation Board
   * [[:​resources:​eval:​dpg:​hsdac-sdp-h1|SDP-H1]] (EVAL-SDP-CH1Z) or [[:​resources:​eval:​ads7-v2|ADS7-V2EBZ]] ​   * [[:​resources:​eval:​dpg:​hsdac-sdp-h1|SDP-H1]] (EVAL-SDP-CH1Z) or [[:​resources:​eval:​ads7-v2|ADS7-V2EBZ]] ​
-  * Evaluation Kit 
   * [[adi>​AD-DAC-FMC]]-ADP High-Speed DAC Evaluation Board to FMC Adaptor Board   * [[adi>​AD-DAC-FMC]]-ADP High-Speed DAC Evaluation Board to FMC Adaptor Board
   * 5Vdc 2A Power Supply   * 5Vdc 2A Power Supply
Line 63: Line 62:
      * If using **ADS7-V2**,​ All three indicators should light up as shown in figure 3b. <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9739a_ace_chip_sdp-h1.png?​nolink&​600 |}}//Figure 3a. ACE Initial Board Configuration Wizard for SDP-H1//</​WRAP>​ <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9739a_ace_chip_ads7.png?​nolink&​600 |}}//Figure 3b. ACE Initial Board Configuration Wizard for ADS7-V2//</​WRAP>​      * If using **ADS7-V2**,​ All three indicators should light up as shown in figure 3b. <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9739a_ace_chip_sdp-h1.png?​nolink&​600 |}}//Figure 3a. ACE Initial Board Configuration Wizard for SDP-H1//</​WRAP>​ <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9739a_ace_chip_ads7.png?​nolink&​600 |}}//Figure 3b. ACE Initial Board Configuration Wizard for ADS7-V2//</​WRAP>​
   - Start DPG Lite or DPG Downloader.   - Start DPG Lite or DPG Downloader.
-    * At the **SDP-H1** ​part of the softwarethe device part number ​and **DCO frequency** of around **75 MHz** should be displayed. +    * At the **SDP-H1** ​settingsensure that **Evaluation board** is equal to AD9739A ​and **DCO frequency** of around **75 MHz** should be displayed. 
-    * At the **ADS7-V2** ​part of the softwarethe device part number ​and **DCO frequency** of around **500 MHz** should be displayed.+    * At the **ADS7-V2** ​ ​settingsensure that **Evaluation board** is equal to AD9739A ​and **DCO frequency** of around **500 MHz** should be displayed.
   - In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 4a and 4b.    - In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 4a and 4b. 
     * When using **SDP-H1**, set **Data Rate** to 300 MHz and **Desired Frequency** to 20 MHz.     * When using **SDP-H1**, set **Data Rate** to 300 MHz and **Desired Frequency** to 20 MHz.
resources/eval/dpg/eval-ad9739a.txt · Last modified: 28 Sep 2021 05:11 by Melissa Lorenz Lacanlale