This is an old revision of the document!
Documentation and software updates for using the AD9114/AD9115/AD9116/AD9117/AD9714/AD9715/AD9716/AD9717 Evaluation Boards are included in self-extracting update files. Documentation can also be downloaded individually below.
Download the AD971X/AD911X Update
The Data Pattern Generator (DPG) is a bench-top instrument for driving vectors into high-speed digital-to-analog converters. The DPG connects to a USB on a PC and allows a user to download a vector from the PC into the internal memory of the DPG. Once downloaded, the vector can be played out to an attached evaluation board for a specific DAC at full speed. This allows for rapid evaluation of the DAC with both generic and custom-generated test data.
For more information on the DPG line of pattern generators and software: