Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:dpg:eval-ad9146 [01 Aug 2022 07:10] – [Preface] Shine Cabatanresources:eval:dpg:eval-ad9146 [16 Jun 2023 05:53] (current) John Marco Mina
Line 52: Line 52:
   - Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J1, and the DAC output from J5 or J9 to a signal/spectrum analyzer. Connect the evaluation board to PC via USB and to a 5Vdc 2A power supply via banana plug cables. Refer to Figures 1a and 1b.   - Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J1, and the DAC output from J5 or J9 to a signal/spectrum analyzer. Connect the evaluation board to PC via USB and to a 5Vdc 2A power supply via banana plug cables. Refer to Figures 1a and 1b.
      * If using **SDP-H1**, set clock input to **100 MHz and 0 dBm**. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart.      * If using **SDP-H1**, set clock input to **100 MHz and 0 dBm**. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart.
-     * If using **ADS7-V2**, set the clock input to **500 MHz and 0 dBm**. Connect ADS-V2 to PC via USB and to a 12V 60W AC/DC power supply. Switch the board ON using S1 beside the connector for 12V supply.+     * If using **ADS7-V2**, set the clock input to **500 MHz and 0 dBm**. Connect ADS7-V2 to PC via USB and to a 12V 60W AC/DC power supply. Switch the board ON using S1 beside the connector for 12V supply.
   - Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9146 evaluation board. Apply the configuration wizard settings shown in Figure 2a for SDP-H1 and in Figure 2b for ADS7-V2. <WRAP centeralign>{{ :resources:eval:dpg:ad9146_ace_sdp-h1.png?600 }}//Figure 2a. ACE Initial Configuration Wizard when using SDP-H1//</WRAP><WRAP centeralign>{{ :resources:eval:dpg:ad9146_ace_ads7-v2.png?600 }}//Figure 2b. ACE Initial Configuration Wizard when using ADS7-V2//</WRAP>   - Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9146 evaluation board. Apply the configuration wizard settings shown in Figure 2a for SDP-H1 and in Figure 2b for ADS7-V2. <WRAP centeralign>{{ :resources:eval:dpg:ad9146_ace_sdp-h1.png?600 }}//Figure 2a. ACE Initial Configuration Wizard when using SDP-H1//</WRAP><WRAP centeralign>{{ :resources:eval:dpg:ad9146_ace_ads7-v2.png?600 }}//Figure 2b. ACE Initial Configuration Wizard when using ADS7-V2//</WRAP>
      * If using **SDP-H1**, set **DAC frequency** to 100 MHz, **Interpolation** to 2x and **Data Format** to binary format.      * If using **SDP-H1**, set **DAC frequency** to 100 MHz, **Interpolation** to 2x and **Data Format** to binary format.
Line 62: Line 62:
   - In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 3a and 3b. The data rate in DPG software should be equal to the data rate in ACE.   - In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 3a and 3b. The data rate in DPG software should be equal to the data rate in ACE.
     * When using SDP-H1, set **Data Rate** to 50 MHz and **Desired Frequency** to 10 MHz.     * When using SDP-H1, set **Data Rate** to 50 MHz and **Desired Frequency** to 10 MHz.
-    * When using ADS-V2, set **Data Rate** to 250 MHz and **Desired Frequency** to 21 MHz.+    * When using ADS7-V2, set **Data Rate** to 250 MHz and **Desired Frequency** to 21 MHz.
   - Continuing on setting up DPG Lite or DPG Downloader, set **DAC resolution** to 16 bits. Check off the **Generate Complex Data (I & Q)** box.\\ <WRAP centeralign>{{ :resources:eval:dpg:ad9146_dpg-lite_sdp-h1.png?600 |}}//Figure 3a. DPG Lite session for SDP-H1//</WRAP><WRAP centeralign>{{ :resources:eval:dpg:ad9146_dpg-lite_ads7-v2.png?600 |}}//Figure 3b. DPG Lite session for ADS7-V2//</WRAP>   - Continuing on setting up DPG Lite or DPG Downloader, set **DAC resolution** to 16 bits. Check off the **Generate Complex Data (I & Q)** box.\\ <WRAP centeralign>{{ :resources:eval:dpg:ad9146_dpg-lite_sdp-h1.png?600 |}}//Figure 3a. DPG Lite session for SDP-H1//</WRAP><WRAP centeralign>{{ :resources:eval:dpg:ad9146_dpg-lite_ads7-v2.png?600 |}}//Figure 3b. DPG Lite session for ADS7-V2//</WRAP>
   - Select the in-phase tone from the **I Data Vector** pulldown menu and the quadrature tone from the **Q Data Vector** pulldown menu.   - Select the in-phase tone from the **I Data Vector** pulldown menu and the quadrature tone from the **Q Data Vector** pulldown menu.
resources/eval/dpg/eval-ad9146.txt · Last modified: 16 Jun 2023 05:53 by John Marco Mina