This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:dpg:eval-ad9146 [01 Aug 2022 07:10] – [Preface] Shine Cabatan | resources:eval:dpg:eval-ad9146 [16 Jun 2023 05:53] (current) – John Marco Mina | ||
---|---|---|---|
Line 52: | Line 52: | ||
- Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J1, and the DAC output from J5 or J9 to a signal/ | - Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J1, and the DAC output from J5 or J9 to a signal/ | ||
* If using **SDP-H1**, set clock input to **100 MHz and 0 dBm**. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart. | * If using **SDP-H1**, set clock input to **100 MHz and 0 dBm**. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart. | ||
- | * If using **ADS7-V2**, | + | * If using **ADS7-V2**, |
- Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9146 evaluation board. Apply the configuration wizard settings shown in Figure 2a for SDP-H1 and in Figure 2b for ADS7-V2. <WRAP centeralign> | - Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9146 evaluation board. Apply the configuration wizard settings shown in Figure 2a for SDP-H1 and in Figure 2b for ADS7-V2. <WRAP centeralign> | ||
* If using **SDP-H1**, set **DAC frequency** to 100 MHz, **Interpolation** to 2x and **Data Format** to binary format. | * If using **SDP-H1**, set **DAC frequency** to 100 MHz, **Interpolation** to 2x and **Data Format** to binary format. | ||
Line 62: | Line 62: | ||
- In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 3a and 3b. The data rate in DPG software should be equal to the data rate in ACE. | - In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 3a and 3b. The data rate in DPG software should be equal to the data rate in ACE. | ||
* When using SDP-H1, set **Data Rate** to 50 MHz and **Desired Frequency** to 10 MHz. | * When using SDP-H1, set **Data Rate** to 50 MHz and **Desired Frequency** to 10 MHz. | ||
- | * When using ADS-V2, set **Data Rate** to 250 MHz and **Desired Frequency** to 21 MHz. | + | * When using ADS7-V2, set **Data Rate** to 250 MHz and **Desired Frequency** to 21 MHz. |
- Continuing on setting up DPG Lite or DPG Downloader, set **DAC resolution** to 16 bits. Check off the **Generate Complex Data (I & Q)** box.\\ <WRAP centeralign> | - Continuing on setting up DPG Lite or DPG Downloader, set **DAC resolution** to 16 bits. Check off the **Generate Complex Data (I & Q)** box.\\ <WRAP centeralign> | ||
- Select the in-phase tone from the **I Data Vector** pulldown menu and the quadrature tone from the **Q Data Vector** pulldown menu. | - Select the in-phase tone from the **I Data Vector** pulldown menu and the quadrature tone from the **Q Data Vector** pulldown menu. |