Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:dpg:dpg1 [18 Jul 2012 15:12] – Approved Jason Coutermarshresources:eval:dpg:dpg1 [03 Jan 2021 22:11] (current) – fix links Robin Getz
Line 12: Line 12:
 ===== Installation ===== ===== Installation =====
   * If you don't have Java installed, install it from www.java.com   * If you don't have Java installed, install it from www.java.com
-  * Run the [[http://www.analog.com/static/imported-files/eval_boards/setup.exe|setup.exe]] file+  * Run the [[adi>static/imported-files/eval_boards/setup.exe|setup.exe]] file
 ===== After Installation ===== ===== After Installation =====
   * Power up the DPG with the included power supply (5V, 8A minimum)   * Power up the DPG with the included power supply (5V, 8A minimum)
Line 55: Line 55:
 The SPI port provides a direct interface with the DAC. The SPI port provides a direct interface with the DAC.
  
-<note>**Note: Clock And Data Alignment** When running in LVDS HS mode, the firmware executes a clock tuning algorithm based on the mode settings (aligned or centered). This algorithm is triggered when data playback is started. +<WRAP round help>**Note: Clock And Data Alignment** When running in LVDS HS mode, the firmware executes a clock tuning algorithm based on the mode settings (aligned or centered). This algorithm is triggered when data playback is started. 
  
 The hardware implementation for the tuning is based on Programmable Delay Controllers, which are unfortunately susceptible to temperature variations. What this means is that if a playback is started when the device is still cold, the clock and data may eventually be misaligned as the board heats up. The hardware implementation for the tuning is based on Programmable Delay Controllers, which are unfortunately susceptible to temperature variations. What this means is that if a playback is started when the device is still cold, the clock and data may eventually be misaligned as the board heats up.
  
 This may be corrected by either restarting the playback or from the “Re-Tune” button in the Tuning dialog. This may be corrected by either restarting the playback or from the “Re-Tune” button in the Tuning dialog.
-</note>+</WRAP>
  
 ====== Hardware ====== ====== Hardware ======
resources/eval/dpg/dpg1.txt · Last modified: 03 Jan 2021 22:11 by Robin Getz