Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:dpg:ad9739a-ebz [12 Jun 2017 22:34]
bailsmeyer [ACE Software]
resources:eval:dpg:ad9739a-ebz [13 Jun 2017 23:05]
bailsmeyer [Software]
Line 17: Line 17:
  
 ==== Software ==== ==== Software ====
-The AD9739A-EBZ is designed to receive data from a DPG2. The DAC Software Suite, plus the AD9739A Update, is required for evaluation. The DAC Software Suite is included on the Evaluation Board CD, or can be downloaded from the DPG web site at http://​www.analog.com/​dpg. This will install DPGDownloader (for loading vectors into the DPG2) and the AD9739A SPI application. However, ACE, a newer evaluation software from ADI, is the preferred evaluation software over the SPI application. It can be downloaded from the ACE website at https://​wiki.analog.com/​resources/​tools-software/​ace. Also required is the ACE plug-in for the evaluation board, which is available for download on the AD9739A eval webpage in the software section at http://​www.analog.com/​en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​EVAL-AD9739A.html#​eb-relatedsoftware. ​+The AD9739A-EBZ is designed to receive data from a DPG2. The DAC Software Suite, plus the AD9739A Update, is required for evaluation. The DAC Software Suite is included on the Evaluation Board CD, or can be downloaded from the DPG web site at http://​www.analog.com/​dpg. This will install DPGDownloader (for loading vectors into the DPG2) and the legacy ​AD9739A SPI application. However, ACE, a newer evaluation software from ADI, is the preferred evaluation software over the SPI application. It can be downloaded from the ACE website at https://​wiki.analog.com/​resources/​tools-software/​ace. Also required is the ACE plug-in for the evaluation board, which is available for download on the AD9739A eval webpage in the software section at http://​www.analog.com/​en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​EVAL-AD9739A.html#​eb-relatedsoftware. ​
  
 ==== Hardware Setup ==== ==== Hardware Setup ====
resources/eval/dpg/ad9739a-ebz.txt · Last modified: 13 Jun 2017 23:05 by bailsmeyer