Wiki

This version is outdated by a newer approved version.DiffThis version (20 Sep 2021 03:29) was approved by Melissa Lorenz Lacanlale.The Previously approved version (14 Sep 2021 10:33) is available.Diff

This is an old revision of the document!


EVALUATING THE AD9739 RF DIGITAL-TO-ANALOG CONVERTER

Preface

This user guide describes both the hardware and software setup needed to acquire data capture from AD9739-R2-EBZ evaluation board to characterize AD9739 14-Bit, 2.5 GSPS, RF Digital-to-Analog Converter.

This guide shows how AD9739-R2-EBZ works with SDP-H1 or ADS7-V2 controller board developed by Analog Devices. Link to the previous user guide document is provided for customers who still have the DPG3 controller board.

Typical Setup

Figure 1a. EVAL-AD9739 Setup with SDP-H1

Figure 1b. EVAL-AD9739 Setup with ADS7-V2

Tip: Click on any picture in this guide to open an enlarged version.

Helpful Files:

Software Needed:

Hardware Needed:

  • AD9739-R2-EBZ Evaluation Board
  • SDP-H1 (EVAL-SDP-CH1Z) or ADS7-V2EBZ
  • Evaluation Kit
  • AD-DAC-FMC-ADP High-Speed DAC Evaluation Board to FMC Adaptor Board
  • 5Vdc 2A Power Supply
  • PC with ACE and DPG Lite Software Applications
  • High-Frequency Continuous Wave Generator
  • Signal/Spectrum Analyzer
  • USB-A to USB-Mini Cable
  • (2) SMA Cables
  • Power Supply to SMA cable
  • The following are included in SDP-H1 Evaluation Kit:
    • 12Vdc 2.5A Wall Wart
    • USB-A to USB-Mini Cable
  • The following are included in ADS7-V2 Evaluation Kit:
    • 12V 60W AC/DC Power Supply
    • Power Cord
    • USB-A to USB-B Cable

Quick Start Guide

  1. Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J3, and the DAC output from J1 to a signal/spectrum analyzer. Connect the evaluation board to PC via USB and a 5Vdc 2A power supply to J17. Refer to Figures 1a and 1b.
    • If using SDP-H1, set clock input to 300 MHz and 0 dBm. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart.
    • If using ADS7-V2, set the clock input to 2 GHz and 0 dBm. Connect ADS-V2 to PC via USB and to a 12V 60W AC/DC power supply. Switch the board ON using S1 beside the connector for 12V supply.
  2. Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9739 evaluation board. From the AD9739-EBZ tab, Click “Run Example Startup Routine (Sync Disabled)”. The MU Controller Locked indicator should light up as shown in figure 2.

    Figure 2. ACE Initial Board Configuration Wizard

  3. Double click the AD9739 Box to open chip view. The DLL_LOCKED indicator should be enabled as shown in figure 3.

    Figure 3. ACE Initial Chip Configuration Wizard

  4. Start DPG Lite or DPG Downloader.
    • At the SDP-H1 part of the software, the device part number and DCO frequency of around 75 MHz should be displayed.
    • At the ADS7-V2 part of the software, the device part number and DCO frequency of around 500 MHz should be displayed.
  5. In DPG Lite or DPG Downloader, from the Add Generator Waveforms pulldown menu, select Single Tone and apply the settings as shown in Figures 4a and 4b.
    • When using SDP-H1, set Data Rate to 300 MHz and Desired Frequency to 20 MHz.
    • When using ADS-V2, set Data Rate to 2 GHz and Desired Frequency to 180 MHz.
  6. Continuing on setting up DPG Lite or DPG Downloader, set DAC resolution to 14 bits. Check off the Unsigned Data box.
  7. Select the Single Tone from the Data Vector pulldown menu

    Figure 4a. DPG Lite session for SDP-H1

    Figure 4b. DPG Lite session for ADS7-V2

  8. Press the download arrow and then the play button. The FFT plots similar to Figures 5a and 5b should appear in the signal/spectrum analyzer.

    Figure 5a. EVAL-AD9739 FFT for Data Rate = 300 MHz, Fout = 20 MHz using SDP-H1

    Figure 5b. EVAL-AD9739 FFT for Data Rate = 2 GHz, Fout = 180 MHz using AD7-V2

Troubleshooting

This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur:

  • Check the supply voltage of the evaluation board. Voltage rail should be 3.3V.
  • Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up.
  • Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 should lit up.
  • Power cycle both the SDP-H1/ADS7-V2 and the AD9739 evaluation board.
  • Check on the Spectrum Analyzer if the DAC clock inputs are properly driven. For 300MHz clock using SDP-H1, the spectrum analyzer should detect a weak signal at 300MHz. For 2GHz clock using ADS7-V2, the spectrum analyzer should detect a weak signal at 2GHz. If not detected, check properly the clock source and connections.
  • Disconnect and reconnect the SDP-H1 /ADS7-V2 and AD9739 evaluation board. Reopen DPG Lite software.
resources/eval/dpg/ad9739-ebz.1632101337.txt.gz · Last modified: 20 Sep 2021 03:28 by Melissa Lorenz Lacanlale