This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision Next revision Both sides next revision | ||
resources:eval:dpg:ad9739-ebz [20 Sep 2021 09:27] Melissa Lorenz Lacanlale Update to SDPH1 and ADSV7 |
resources:eval:dpg:ad9739-ebz [21 Sep 2021 10:16] Melissa Lorenz Lacanlale [Quick Start Guide] |
||
---|---|---|---|
Line 56: | Line 56: | ||
=====Quick Start Guide===== | =====Quick Start Guide===== | ||
- | - Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J3, and the DAC output from J1 to a signal/spectrum analyzer. Connect the evaluation board to PC via USB and a 5Vdc 2A power supply to J17. Refer to Figures 1a and 1b. | + | - Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J3, and the DAC output from J1 to a signal/spectrum analyzer. Connect the evaluation board to PC via USB, a 5Vdc 2A power supply to J17. Refer to Figures 1a and 1b. |
* If using **SDP-H1**, set clock input to **300 MHz and 0 dBm**. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart. | * If using **SDP-H1**, set clock input to **300 MHz and 0 dBm**. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart. | ||
* If using **ADS7-V2**, set the clock input to **2 GHz and 0 dBm**. Connect ADS-V2 to PC via USB and to a 12V 60W AC/DC power supply. Switch the board ON using S1 beside the connector for 12V supply. | * If using **ADS7-V2**, set the clock input to **2 GHz and 0 dBm**. Connect ADS-V2 to PC via USB and to a 12V 60W AC/DC power supply. Switch the board ON using S1 beside the connector for 12V supply. | ||
Line 63: | Line 63: | ||
* If using **ADS7-V2**, The first three indicators should light up as shown in figure 2b. <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ace_boardview.png?nolink&600 |}}//Figure 2a. ACE Initial Board Configuration Wizard for SDP-H1//</WRAP> <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ads7_ace_boardview.png?nolink&600 |}}//Figure 2a. ACE Initial Board Configuration Wizard for ADS7-V2//</WRAP> | * If using **ADS7-V2**, The first three indicators should light up as shown in figure 2b. <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ace_boardview.png?nolink&600 |}}//Figure 2a. ACE Initial Board Configuration Wizard for SDP-H1//</WRAP> <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ads7_ace_boardview.png?nolink&600 |}}//Figure 2a. ACE Initial Board Configuration Wizard for ADS7-V2//</WRAP> | ||
- Double click the AD9739 Box to open chip view. | - Double click the AD9739 Box to open chip view. | ||
- | * If using **SDP-H1**, The DLL_LOCKED indicator should be enabled as shown in figure 3a. | + | * If using **SDP-H1**, The DLL_LOCKED indicator should light up as shown in figure 3a. |
* If using **ADS7-V2**, All three indicators should light up as shown in figure 3b. <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ace_chipview.png?nolink&600 |}}//Figure 3a. ACE Initial Board Configuration Wizard for SDP-H1//</WRAP> <WRAP centeralign>{{ :resources:eval:dpg:ad9739_adsv7_ace_chipview.png?nolink&600 |{{ :resources:eval:dpg:ad9739_ads7_ace_boardview.png?nolink&600 |}}//Figure 3b. ACE Initial Board Configuration Wizard for ADS7-V2//</WRAP> | * If using **ADS7-V2**, All three indicators should light up as shown in figure 3b. <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ace_chipview.png?nolink&600 |}}//Figure 3a. ACE Initial Board Configuration Wizard for SDP-H1//</WRAP> <WRAP centeralign>{{ :resources:eval:dpg:ad9739_adsv7_ace_chipview.png?nolink&600 |{{ :resources:eval:dpg:ad9739_ads7_ace_boardview.png?nolink&600 |}}//Figure 3b. ACE Initial Board Configuration Wizard for ADS7-V2//</WRAP> | ||
- Start DPG Lite or DPG Downloader. | - Start DPG Lite or DPG Downloader. | ||
Line 78: | Line 78: | ||
=====Troubleshooting===== | =====Troubleshooting===== | ||
This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur: | This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur: | ||
- | * Check the supply voltage of the evaluation board. Voltage rail should be 3.3V. | + | * Check if the Voltage supply test points of the evaluation board has the correct value. |
* Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up. | * Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up. | ||
* Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 should lit up. | * Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 should lit up. |