This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:dpg:ad9739-ebz [20 Sep 2021 09:27] – Update to SDPH1 and ADSV7 Melissa Lorenz Lacanlale | resources:eval:dpg:ad9739-ebz [20 Sep 2021 10:10] – update troubleshooting voltage supplies Melissa Lorenz Lacanlale | ||
---|---|---|---|
Line 63: | Line 63: | ||
* If using **ADS7-V2**, | * If using **ADS7-V2**, | ||
- Double click the AD9739 Box to open chip view. | - Double click the AD9739 Box to open chip view. | ||
- | * If using **SDP-H1**, The DLL_LOCKED indicator should | + | * If using **SDP-H1**, The DLL_LOCKED indicator should |
* If using **ADS7-V2**, | * If using **ADS7-V2**, | ||
- Start DPG Lite or DPG Downloader. | - Start DPG Lite or DPG Downloader. | ||
Line 78: | Line 78: | ||
=====Troubleshooting===== | =====Troubleshooting===== | ||
This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur: | This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur: | ||
- | * Check the supply | + | * Check if the Voltage |
* Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up. | * Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up. | ||
* Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 should lit up. | * Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 should lit up. |