Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Last revision Both sides next revision
resources:eval:dpg:ad9739-ebz [20 Sep 2021 03:28]
Melissa Lorenz Lacanlale Update to SDPH1 and ADSV7
resources:eval:dpg:ad9739-ebz [21 Sep 2021 10:16]
Melissa Lorenz Lacanlale [Quick Start Guide]
Line 56: Line 56:
  
 =====Quick Start Guide===== =====Quick Start Guide=====
-  - Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J3, and the DAC output from J1 to a signal/​spectrum analyzer. Connect the evaluation board to PC via USB and a 5Vdc 2A power supply to J17. Refer to Figures 1a and 1b.+  - Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J3, and the DAC output from J1 to a signal/​spectrum analyzer. Connect the evaluation board to PC via USBa 5Vdc 2A power supply to J17. Refer to Figures 1a and 1b.
      * If using **SDP-H1**, set clock input to **300 MHz and 0 dBm**. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart.      * If using **SDP-H1**, set clock input to **300 MHz and 0 dBm**. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart.
      * If using **ADS7-V2**,​ set the clock input to **2 GHz and 0 dBm**. Connect ADS-V2 to PC via USB and to a 12V 60W AC/DC power supply. Switch the board ON using S1 beside the connector for 12V supply.      * If using **ADS7-V2**,​ set the clock input to **2 GHz and 0 dBm**. Connect ADS-V2 to PC via USB and to a 12V 60W AC/DC power supply. Switch the board ON using S1 beside the connector for 12V supply.
-  - Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9739 evaluation board. From the AD9739-EBZ tab, Click **“Run Example Startup Routine (Sync Disabled)”**. ​The **MU Controller Locked** ​indicator ​should light up as shown in figure ​2 <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9739_ace_boardview.png?​nolink&​600 |}}//​Figure ​2. ACE Initial Board Configuration Wizard //</​WRAP>​ +  - Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9739 evaluation board. From the AD9739-EBZ tab, Click **“Run Example Startup Routine (Sync Disabled)”**. ​ 
-  - Double click the AD9739 Box to open chip view. The **DLL_LOCKED** indicator should ​be enabled ​as shown in figure ​3.<WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9739_ace_chipview.png?​nolink&​600 |}}//​Figure ​3. ACE Initial ​Chip  ​Configuration Wizard//</​WRAP>​+     If using **SDP-H1**, The MU Controller Locked ​indicator should light up as shown in figure 2a. 
 +     If using **ADS7-V2**, The first three indicators ​should light up as shown in figure ​2b. <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9739_ace_boardview.png?​nolink&​600 |}}//​Figure ​2a. ACE Initial Board Configuration Wizard ​for SDP-H1//</​WRAP>​ <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9739_ads7_ace_boardview.png?​nolink&​600 |}}//Figure 2a. ACE Initial Board Configuration Wizard for ADS7-V2//</​WRAP>​ 
 +  - Double click the AD9739 Box to open chip view.  
 +     If using **SDP-H1**, The DLL_LOCKED ​indicator should ​light up as shown in figure 3a. 
 +     * If using **ADS7-V2**,​ All three indicators should light up as shown in figure ​3b. <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9739_ace_chipview.png?​nolink&​600 |}}//​Figure ​3a. ACE Initial ​Board Configuration Wizard ​for SDP-H1//</​WRAP>​ <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9739_adsv7_ace_chipview.png?​nolink&​600 |{{ :​resources:​eval:​dpg:​ad9739_ads7_ace_boardview.png?​nolink&​600 |}}//Figure 3b. ACE Initial Board Configuration Wizard for ADS7-V2//</​WRAP>​
   - Start DPG Lite or DPG Downloader.   - Start DPG Lite or DPG Downloader.
     * At the SDP-H1 part of the software, the device part number and **DCO frequency** of around **75 MHz** should be displayed.     * At the SDP-H1 part of the software, the device part number and **DCO frequency** of around **75 MHz** should be displayed.
Line 74: Line 78:
 =====Troubleshooting===== =====Troubleshooting=====
 This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur: This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur:
-  * Check the supply ​voltage ​of the evaluation board. Voltage rail should be 3.3V.+  * Check if the Voltage ​supply ​test points ​of the evaluation board has the correct value
   * Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up.   * Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up.
   * Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 should lit up.   * Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 should lit up.
resources/eval/dpg/ad9739-ebz.txt · Last modified: 28 Sep 2021 07:26 by Melissa Lorenz Lacanlale