This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:dpg:ad917x-fmc-ebz [24 Jun 2020 17:46] – [KCU105 Setup] Eric Chaykovsky | resources:eval:dpg:ad917x-fmc-ebz [09 Feb 2022 21:19] (current) – [ADS7/ADS8-V1 Setup] Arik Landsman | ||
---|---|---|---|
Line 3: | Line 3: | ||
* AD9171-FMC-EBZ or AD9172-FMC-EBZ or AD9173-FMC-EBZ or AD9174-FMC-EBZ or AD9175-FMC-EBZ or AD9176-FMC-EBZ Evaluation Board | * AD9171-FMC-EBZ or AD9172-FMC-EBZ or AD9173-FMC-EBZ or AD9174-FMC-EBZ or AD9175-FMC-EBZ or AD9176-FMC-EBZ Evaluation Board | ||
* Mini USB cable | * Mini USB cable | ||
+ | |||
+ | === Additional Components Needed for an ADS7 / ADS8-V1 Evaluation Platform === | ||
+ | * Pattern generator board: ADS7 (up to 13Gbps SERDES) or ADS8-V1 (covers the full AD917x range): [[adi> | ||
**Note: if using the Xilinx KCU105 evaluation kit as a pattern generator, customers will need to purchase the following additional components: | **Note: if using the Xilinx KCU105 evaluation kit as a pattern generator, customers will need to purchase the following additional components: | ||
- | === Additional Components Needed for KCU105 Evaluation Platform === | + | === Additional Components Needed for a KCU105 Evaluation Platform === |
* Xilinx KCU105 Evaluation Kit: http:// | * Xilinx KCU105 Evaluation Kit: http:// | ||
* Cypress FX3 SuperSpeed Explorer Kit (CYUSB3KIT-003): | * Cypress FX3 SuperSpeed Explorer Kit (CYUSB3KIT-003): | ||
Line 53: | Line 56: | ||
- | ==== ADS7/ADS8 Setup ==== | + | ==== ADS7/ADS8-V1 Setup ==== |
+ | <note important> | ||
The Cypress FX3 and interconnect board are not needed if the ADS7 or ADS8 board is used for data pattern generation. The hardware setup configuration when using the ADS7/ADS8 is as follows: | The Cypress FX3 and interconnect board are not needed if the ADS7 or ADS8 board is used for data pattern generation. The hardware setup configuration when using the ADS7/ADS8 is as follows: | ||
- Connect the AD917x-FMC-EBZ board to the FMC connector on the ADS7 or ADS8. | - Connect the AD917x-FMC-EBZ board to the FMC connector on the ADS7 or ADS8. | ||
Line 62: | Line 65: | ||
{{ : | {{ : | ||
- | Figure 3. Evaluation Board Kit Components Hardware Connection Setup with ADS8 | + | Figure 3. Evaluation Board Kit Components Hardware Connection Setup with ADS8-V1 |
==== KCU105 Setup ==== | ==== KCU105 Setup ==== | ||
Line 120: | Line 123: | ||
=== Using KCU105 with DPG Downloader === | === Using KCU105 with DPG Downloader === | ||
- | The KCU-105 | + | The KCU105 |
{{ : | {{ : | ||
Figure 2. KCU105 DIP Switch Settings for Loading Image from Micro-SD Card | Figure 2. KCU105 DIP Switch Settings for Loading Image from Micro-SD Card | ||
- | Once these steps are complete, the KCU105 board can be powered on and plugged into the USB ports on the host PC. This step only needs to be done once in order to set up the FPGA board properly for any future use with DPGDownloader software. | + | Once these steps are complete, the KCU105 board can be powered on and plugged into the USB ports on the host PC. After powering on the KCU105, wait approximately 10 seconds so that the KCU105 has adequate time to load the FPGA image. If the KCU105' |
==== Other FPGA Development Kits==== | ==== Other FPGA Development Kits==== | ||
Line 136: | Line 139: | ||
The outputs of the AD917x can be captured at the SMA connectors: J1 for DAC0; J2 for DAC1; and J3 for CLKOUT. | The outputs of the AD917x can be captured at the SMA connectors: J1 for DAC0; J2 for DAC1; and J3 for CLKOUT. | ||
+ | |||
+ | Some applications may be more sensitive to clock spurious. To prevent any spurious coupling from the onboard HMC7044 onto the AD917x output, the HMC7044 may be kept in reset: | ||
+ | |||
+ | - reset the board in ACE (Reset Board button in the " | ||
+ | - in the Wizard, under Eval System Option select chip to configure: " | ||
+ | - Under DC Test Mode, select the option " | ||
+ | - Under SERDES Interface, set the link mode and interpolation (this will apply a clock to the corresponding datapaths. E.g. dual-link to enable both datapath0 and datapath1, that would feed DAC0 and DAC1 respectively) | ||
+ | - Under Clock frequencies, | ||
Line 236: | Line 247: | ||
The raw macro file will be saved using ACE syntax, which is not easily readable. To remedy this, the ACE software download includes the Macro to Hex Conversion Tool. The user can choose to include or exclude register write, reads, and/or comments in the conversion. The file pathways for the source and save paths should be the same, except that one should be an .acemacro file and the other should be a .txt file. The “Convert” button converts and opens the converted text file, which is easier to read. The conversion tool can also convert back to an .acemacro file if desired. The Macro to Hex converter tool is located in the start menu under "All Programs" | The raw macro file will be saved using ACE syntax, which is not easily readable. To remedy this, the ACE software download includes the Macro to Hex Conversion Tool. The user can choose to include or exclude register write, reads, and/or comments in the conversion. The file pathways for the source and save paths should be the same, except that one should be an .acemacro file and the other should be a .txt file. The “Convert” button converts and opens the converted text file, which is easier to read. The conversion tool can also convert back to an .acemacro file if desired. The Macro to Hex converter tool is located in the start menu under "All Programs" | ||
+ | <note important> | ||
<WRAP column 40%> | <WRAP column 40%> | ||
{{ : | {{ : |