Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:dpg:ad917x-fmc-ebz [24 Sep 2021 13:39] – [ACE Macro Recorder Tool] Ciaran Wattersonresources:eval:dpg:ad917x-fmc-ebz [09 Feb 2022 21:19] (current) – [ADS7/ADS8-V1 Setup] Arik Landsman
Line 3: Line 3:
   * AD9171-FMC-EBZ or AD9172-FMC-EBZ or AD9173-FMC-EBZ or AD9174-FMC-EBZ or AD9175-FMC-EBZ or AD9176-FMC-EBZ Evaluation Board   * AD9171-FMC-EBZ or AD9172-FMC-EBZ or AD9173-FMC-EBZ or AD9174-FMC-EBZ or AD9175-FMC-EBZ or AD9176-FMC-EBZ Evaluation Board
   * Mini USB cable   * Mini USB cable
 +
 +=== Additional Components Needed for an ADS7 / ADS8-V1 Evaluation Platform ===
 +  * Pattern generator board: ADS7 (up to 13Gbps SERDES) or ADS8-V1 (covers the full AD917x range): [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/ADS8-V1EBZ.html]]
  
 **Note: if using the Xilinx KCU105 evaluation kit as a pattern generator, customers will need to purchase the following additional components:** **Note: if using the Xilinx KCU105 evaluation kit as a pattern generator, customers will need to purchase the following additional components:**
  
-=== Additional Components Needed for KCU105 Evaluation Platform ===+=== Additional Components Needed for KCU105 Evaluation Platform ===
   * Xilinx KCU105 Evaluation Kit: http://www.xilinx.com/products/boards-and-kits/kcu105.html   * Xilinx KCU105 Evaluation Kit: http://www.xilinx.com/products/boards-and-kits/kcu105.html
   * Cypress FX3 SuperSpeed Explorer Kit (CYUSB3KIT-003): https://www.cypress.com/documentation/development-kitsboards/cyusb3kit-003-ez-usb-fx3-superspeed-explorer-kit   * Cypress FX3 SuperSpeed Explorer Kit (CYUSB3KIT-003): https://www.cypress.com/documentation/development-kitsboards/cyusb3kit-003-ez-usb-fx3-superspeed-explorer-kit
Line 53: Line 56:
  
  
-==== ADS7/ADS8 Setup ==== +==== ADS7/ADS8-V1 Setup ==== 
-<note important>NOTE: The ADS8 is preferred over the ADS7which is limited to 13Gbps JESD Lane rate.</note>+<note important>NOTE: The ADS8-V1 covers the full range of the SERDES (JESD204B) lane rate of the deviceup-to 16Gbps. The ADS7 is limited to 13Gbps Lane rate, and may be a good economical alternative for users interested to operate at lower datarates.</note>
 The Cypress FX3 and interconnect board are not needed if the ADS7 or ADS8 board is used for data pattern generation. The hardware setup configuration when using the ADS7/ADS8 is as follows: The Cypress FX3 and interconnect board are not needed if the ADS7 or ADS8 board is used for data pattern generation. The hardware setup configuration when using the ADS7/ADS8 is as follows:
   - Connect the AD917x-FMC-EBZ board to the FMC connector on the ADS7 or ADS8.   - Connect the AD917x-FMC-EBZ board to the FMC connector on the ADS7 or ADS8.
Line 62: Line 65:
  
 {{ :resources:eval:dpg:ad9172:figure3_ads8_ad9172fmc.png?direct |}} {{ :resources:eval:dpg:ad9172:figure3_ads8_ad9172fmc.png?direct |}}
-Figure 3. Evaluation Board Kit Components Hardware Connection Setup with ADS8+Figure 3. Evaluation Board Kit Components Hardware Connection Setup with ADS8-V1
  
 ==== KCU105 Setup ==== ==== KCU105 Setup ====
resources/eval/dpg/ad917x-fmc-ebz.txt · Last modified: 09 Feb 2022 21:19 by Arik Landsman