This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:dpg:ad917x-fmc-ebz [19 Nov 2020 23:16] – [NCO-only Mode ("DC Test Mode") Without ADS7/ADS8/KCU105] Arik Landsman | resources:eval:dpg:ad917x-fmc-ebz [24 Sep 2021 13:35] – [ADS7/ADS8 Setup] Hint that ADS8 is better than ADS7 Ciaran Watterson | ||
---|---|---|---|
Line 54: | Line 54: | ||
==== ADS7/ADS8 Setup ==== | ==== ADS7/ADS8 Setup ==== | ||
+ | <note important> | ||
The Cypress FX3 and interconnect board are not needed if the ADS7 or ADS8 board is used for data pattern generation. The hardware setup configuration when using the ADS7/ADS8 is as follows: | The Cypress FX3 and interconnect board are not needed if the ADS7 or ADS8 board is used for data pattern generation. The hardware setup configuration when using the ADS7/ADS8 is as follows: | ||
- Connect the AD917x-FMC-EBZ board to the FMC connector on the ADS7 or ADS8. | - Connect the AD917x-FMC-EBZ board to the FMC connector on the ADS7 or ADS8. |