Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision Both sides next revision
resources:eval:dpg:ad9154-fmc-ebz [27 Feb 2015 23:00]
Larry Welch
resources:eval:dpg:ad9154-fmc-ebz [27 Feb 2015 23:21]
Michael Fowler Spelling
Line 26: Line 26:
 The PC software is included in the CD shipped with the EVB. The installation will include the software as well as all the AD9154 EVB files including schematic, board layout, datasheet, this quick start guide and other files. ​ The PC software is included in the CD shipped with the EVB. The installation will include the software as well as all the AD9154 EVB files including schematic, board layout, datasheet, this quick start guide and other files. ​
 ==== Initial Set-Up ==== ==== Initial Set-Up ====
-1. Install the customer evaluation board software and support files, including ​DPG Dowloader ​and SPIPro GUI on your PC. Follow the instructions in the installation wizard and use the default (recommended) installation settings. ​ \\ \\+1. Install the customer evaluation board software and support files, including ​DPGDownloader ​and SPIPro GUI on your PC. Follow the instructions in the installation wizard and use the default (recommended) installation settings. ​ \\ \\
 2. Plug the AD9154-FMC-EBZ into port FMC_1 of the ADS7 System. Use a USB cable to connect the EVB to your PC and connect the lab equipment to the EVB as shown in Figure 1. \\ \\ 2. Plug the AD9154-FMC-EBZ into port FMC_1 of the ADS7 System. Use a USB cable to connect the EVB to your PC and connect the lab equipment to the EVB as shown in Figure 1. \\ \\
 3. Connect the ADS7 unit to your PC via USB and turn on the ADS7.  \\ \\    3. Connect the ADS7 unit to your PC via USB and turn on the ADS7.  \\ \\   
resources/eval/dpg/ad9154-fmc-ebz.txt · Last modified: 23 Nov 2015 22:10 by Larry Welch