This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:dpg:ad9154-fmc-ebz [27 Feb 2015 22:41] – ert Larry Welch | resources:eval:dpg:ad9154-fmc-ebz [27 Feb 2015 23:21] – Spelling Michael Fowler | ||
---|---|---|---|
Line 26: | Line 26: | ||
The PC software is included in the CD shipped with the EVB. The installation will include the software as well as all the AD9154 EVB files including schematic, board layout, datasheet, this quick start guide and other files. | The PC software is included in the CD shipped with the EVB. The installation will include the software as well as all the AD9154 EVB files including schematic, board layout, datasheet, this quick start guide and other files. | ||
==== Initial Set-Up ==== | ==== Initial Set-Up ==== | ||
- | 1. Install the customer evaluation board software and support files, including | + | 1. Install the customer evaluation board software and support files, including |
2. Plug the AD9154-FMC-EBZ into port FMC_1 of the ADS7 System. Use a USB cable to connect the EVB to your PC and connect the lab equipment to the EVB as shown in Figure 1. \\ \\ | 2. Plug the AD9154-FMC-EBZ into port FMC_1 of the ADS7 System. Use a USB cable to connect the EVB to your PC and connect the lab equipment to the EVB as shown in Figure 1. \\ \\ | ||
3. Connect the ADS7 unit to your PC via USB and turn on the ADS7. \\ \\ | 3. Connect the ADS7 unit to your PC via USB and turn on the ADS7. \\ \\ | ||
Line 71: | Line 71: | ||
<WRAP center> | <WRAP center> | ||
- | {{: | + | {{: |
| Figure 6. DAC Outputs Scope Display | | Figure 6. DAC Outputs Scope Display | ||