Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:dpg:ad9154-ebz [21 Jun 2017 17:06] – Bailey Meyer | resources:eval:dpg:ad9154-ebz [28 Jul 2017 20:46] (current) – Bailey Meyer |
---|
</WRAP> | </WRAP> |
| |
Ensure that the {{:resources:eval:user-guides:connection_icon.png}} button is green in the subsystem image under the “System” tab, as shown in Figure 4. If not, click it, select the AD9136/5, and click //Acquire//. Double click on the subsystem image to reach the board block diagram. | Ensure that the {{:resources:eval:user-guides:connection_icon.png}} button is green in the subsystem image under the “System” tab, as shown in Figure 4. If not, click it, select the AD9154, and click "Acquire." Double click on the subsystem image to reach the board block diagram. |
<WRAP center> | <WRAP center> |
| |
d. Set Data Rate to 750 MHz, Desired Frequency to 112 MHz, Amplitude to -1.0 dBFS, uncheck unsigned, check Generate Complex Data (I&Q). | d. Set Data Rate to 750 MHz, Desired Frequency to 112 MHz, Amplitude to -1.0 dBFS, uncheck unsigned, check Generate Complex Data (I&Q). |
| |
e. Under Data Playback, select I data for DAC 0 and DAC2, and Q data for DAC 1 and DAC3. | e. Under Data Playback, select I data for DAC 0 and DAC2, and Q data for DAC 1 and DAC3. The DPGDownloader settings should resemble Figure 14. |
| |
f. Click Download ({{:resources:eval:dpg:image009.png?direct&|}}) and Play ({{:resources:eval:dpg:image010.png?direct&|}}) in the DPG Downloader screen. The spectrum in Figure 15 will appear on all 4 DAC outputs (J17, J4, J5, and J7), Serial Line Rate will be 7.5Gbps. Figure 16 is a scope capture of the DAC output signal taken on three of the channels. | f. Click Download ({{:resources:eval:dpg:image009.png?direct&|}}) and Play ({{:resources:eval:dpg:image010.png?direct&|}}) in the DPG Downloader screen. The spectrum in Figure 15 will appear on all 4 DAC outputs (J17, J4, J5, and J7), Serial Line Rate will be 7.5Gbps. Figure 16 is a scope capture of the DAC output signal taken on three of the channels. |