This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:dpg:ad9154-ace-fmc-ebz [09 Aug 2022 04:24] – [Typical Setup] Shine Cabatan | resources:eval:dpg:ad9154-ace-fmc-ebz [07 Feb 2023 09:22] (current) – Quick Start Guide Shine Cabatan | ||
---|---|---|---|
Line 5: | Line 5: | ||
This user guide describes both the hardware and software setup needed to acquire data capture from [[adi> | This user guide describes both the hardware and software setup needed to acquire data capture from [[adi> | ||
- | The [[adi> | + | The [[adi> |
===== Typical Setup ===== | ===== Typical Setup ===== | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
- | + | ||
- | <WRAP centeralign> | + | |
<note tip>Tip: Click on any picture in this guide to open an enlarged version.</ | <note tip>Tip: Click on any picture in this guide to open an enlarged version.</ | ||
Line 22: | Line 20: | ||
* [[: | * [[: | ||
* Datasheet: [[adi> | * Datasheet: [[adi> | ||
- | * IBIS Model: [[ibis>ad9152bcpz|AD9152]] | + | * IBIS Model: [[ibis>ad9154bcpz|AD9154]] |
* AMI Model: [[https:// | * AMI Model: [[https:// | ||
- | * Schematic: {{: | + | * Schematic: {{: |
- | * Bill of Materials: {{: | + | * Bill of Materials: {{: |
- | * PCB Gerber Files: {{: | + | * PCB Gerber Files: {{: |
- | * PCB BRD File: {{: | + | * PCB BRD File: {{: |
- | * PCB Layout PDF: {{: | + | * PCB Layout PDF: {{: |
===== Software Needed ===== | ===== Software Needed ===== | ||
Line 36: | Line 34: | ||
* [[adi> | * [[adi> | ||
- | <note important> | + | <note important> |
+ | * Do not install ACE on a computer with DAC Software Suite. | ||
+ | * **Known Issue:** ACE may fail to detect HS-DAC boards, details [[resources: | ||
+ | </ | ||
===== Hardware Needed ===== | ===== Hardware Needed ===== | ||
- | ===== AD9154 | + | * [[adi> |
- | The AD9154 Evaluation Board software runs on the ADI ACE graphical user interface (GUI). ACE is included on the Evaluation board CD. Registers on the AD9154 and AD9516 products are programmed by the ACE software via a USB cable connecting the user’s PC to the AD9154-FMC-EBZ | + | * USB-A to USB-Mini Cable |
- | ===== Hardware Setup ===== | + | |
- | | + | * 12V 60W AC/DC Power Supply |
- | <WRAP center> | + | * Power Cord |
- | {{: | + | |
- | | Figure 1. AD9154-FMC-EBZ Lab Block Diagram | + | |
- | {{:resources: | + | |
- | | Figure 2. Top and Bottom view of AD9154-FMC-EBZ | + | |
- | </WRAP> | + | |
- | A spectrum analyzer should be connected to the EVB SMA connector J4. Connect SMA connectors J5, J14 and J17 of the EVB to an oscilloscope. The evaluation board connects to the ADS7 through the connector P1. The PC should be connected to the EVB using the mini-USB connector XP2. Figure 1 shows a block diagram of the set-up. | + | |
- | + | ||
- | === Clock input: === | + | |
- | A low phase noise high frequency clock source should be connected | + | |
- | | + | |
- | - a reference clock to the AD9154' | + | |
- | + | ||
- | The AD9516 generates the bitrate/40 needed to establish a JESD204B link. If a JESD204B link needs to be established, | + | |
- | + | ||
- | If option #1 is needed, the J1 input is split between the AD9154 and the AD9516. | + | |
- | + | ||
- | If option #2 is needed, AD9154 may receive a reference clock either from the AD9516, as a divided down version of FIN, or directly from the J1 pin. In either case, the J1 input must be high enough to guarantee that the AD9516 can generate a bitrate/40 clock. | + | |
- | + | ||
- | + | ||
- | ===== Getting Started ===== | + | |
- | The PC software is included in the CD shipped | + | |
- | ==== Initial Set-Up ==== | + | |
- | 1. Install the customer evaluation board software and support files, including DPGDownloader and ACE GUI on your PC. Follow the instructions in the installation wizard | + | |
- | 2. Plug the AD9154-FMC-EBZ into port FMC_1 of the ADS7 System. Use a USB cable to connect the EVB to your PC and connect the lab equipment to the EVB as shown in Figure 1. \\ \\ | + | |
- | 3. Connect the ADS7 unit to your PC via USB and turn on the ADS7. \\ \\ | + | |
- | 4. Connect SMA connector J5 to a spectrum analyzer, connect SMA connectors J17, J4 and J14 to an oscilloscope. | + | |
- | ==== Single Tone Demonstration ==== | + | |
- | === Single Tone Demo Lab Bench Configuration Procedure: | + | |
- | + | ||
- | These settings configure the AD9154 to output a 180Mhz 0dbFS sine wave using the ADS7 on all four AD9154 DACs. | + | |
- | + | ||
- | - Configure the hardware according to the hardware set-up instructions given in the Hardware Setup section above. Set the frequency of the DAC clock signal generator to 1500MHz, and the output level to 3dBm. The spectrum analyzer can be configured as shown in Figure 8 with a resolution bandwidth of 300kHz. Choose an Input Attenuation of 22dB. | + | |
- | + | ||
- | <WRAP center> | + | |
- | + | ||
- | {{: | + | |
- | | Figure 3. Initial | + | |
- | </ | + | |
- | === Single Tone Demo Hardware and Software | + | |
- | 1. Run DPG Downloader from Start-> | + | |
- | + | ||
- | <WRAP center> | + | |
- | 2. Open ACE from Start->Analog Devices-> | + | |
- | 3. Press the AD9154 icon and populate the AD9154 initialization wizard as shown in figure 4b, JESD mode 0, Interpolation 2. Leave all other settings in their default state. Press rhe APPLY button. JESD204B PLL lock will turn green as shown in figure 4c. Press the AD9154 icon in the initialization wizard tab. The AD9154 block diagram view will appear populated as shown in figure 4d.\\ \\ | + | |
- | <WRAP center> | + | |
- | {{: | + | |
- | | Figure 4a. Initial ACE page for AD9154-FMC-EBZ | + | |
- | {{: | + | |
- | | Figure 4b. ACE AD9154 Initialization Wizard tab with selections made | | + | |
- | {{: | + | |
- | | Figure 4c. ACE AD9154 Initialization Wizard tab after pressing APPLY | | + | |
- | {{: | + | |
- | | Figure 4d. ACE AD9154 Block Diagram View after Initialization | + | |
- | </WRAP> | + | |
- | 4. In DPG Downloader Window Select Single Tone under the Add Generated Waveforms Tab. Set Data Rate: 750Mhz, Desired Frequency: 180Mhz, Amplitude: 0dbFS, Uncheck Unsigned Data, Check Generate Complex Data (I&Q) | + | |
- | + | ||
- | 5. Select JESD Mode: Mode 0, Select Subclass 0 | + | |
- | + | ||
- | 6. Populate the data playback selections for each DAC output as shown in Figure 5. | + | |
- | + | ||
- | 7. Click Download button | + | |
- | + | ||
- | + | ||
- | <WRAP center> | + | |
- | {{: | + | |
- | | Figure | + | |
- | </ | + | |
- | + | ||
- | 8. Here’s what you will see on DAC0, DAC1, and DAC3 on the scope \\ \\ | + | |
- | + | ||
- | + | ||
- | + | ||
- | <WRAP center> | + | |
- | + | ||
- | + | ||
- | 9. Here is what you will see at the output of DAC2 on the Spectrum Analyzer. | + | |
- | {{: | + | ===== Quick Start Guide ===== |
- | | Figure 6. DAC Output Spectrum Analyzer Display | + | - Attach AD9154-FMC-EBZ onto the FMC connector of ADS7-V2 controller board. Connect the evaluation board to PC via USB, the continuous waveform generator output to J1, one of the DAC outputs to a spectrum/ |
- | </ | + | - Set the frequency of the continuous waveform generator output to **1.5 GHz** and the output level to **+3 dBm**. Enable the output.< |
+ | - Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**, | ||
+ | - Open ACE. The board will automatically be recognized by the software as shown in Figure 3. Otherwise, install the plugin for AD9154 evaluation board by following the steps in this page: [[: | ||
+ | - In ACE, apply the configuration wizard settings enumerated below and shown in Figure 4. JESD204B PLL should lock and the indicator should turn green. | ||
+ | * **Links:** Single Link | ||
+ | * **JESD Mode:** 0 | ||
+ | * **Subclass1: | ||
+ | * **Interpolation: | ||
+ | * **DAC PLL:** False | ||
+ | * **FDAC:** 1.5 GHz <WRAP centeralign> | ||
+ | - In DPG Lite or DPG Downloader, configure single tone waveform generation. From the **Add Generator Waveforms** pulldown menu, select **Single Tone**. Apply the following settings: | ||
+ | * **Data Rate:** 750 MHz | ||
+ | * **Desired Frequency: | ||
+ | * **DAC Resolution: | ||
+ | * **Amplitude: | ||
+ | * **Unsigned Data:** unchecked | ||
+ | * **Generate Complex Data (I & Q):** checked | ||
+ | - In the ADS7-V2 panel in the DPG window, configure **Data Playback** by selecting tones for the DAC outputs from each dropdown menu. Set **JESD Mode** to Mode 0, **Links** to Single, and **Subclass** to 0. <WRAP centeralign> | ||
+ | - Press the download arrow ({{: | ||
- | {{: | ||
- | | |