This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:dpg:ad9154-ace-fmc-ebz [04 Aug 2022 07:56] – [Helpful Files/Links] Shine Cabatan | resources:eval:dpg:ad9154-ace-fmc-ebz [07 Feb 2023 09:22] (current) – Quick Start Guide Shine Cabatan | ||
---|---|---|---|
Line 5: | Line 5: | ||
This user guide describes both the hardware and software setup needed to acquire data capture from [[adi> | This user guide describes both the hardware and software setup needed to acquire data capture from [[adi> | ||
- | The [[adi> | + | The [[adi> |
===== Typical Setup ===== | ===== Typical Setup ===== | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
- | + | ||
- | <WRAP centeralign> | + | |
<note tip>Tip: Click on any picture in this guide to open an enlarged version.</ | <note tip>Tip: Click on any picture in this guide to open an enlarged version.</ | ||
Line 22: | Line 20: | ||
* [[: | * [[: | ||
* Datasheet: [[adi> | * Datasheet: [[adi> | ||
- | * IBIS Model: [[ibis>ad9152bcpz|AD9152]] | + | * IBIS Model: [[ibis>ad9154bcpz|AD9154]] |
* AMI Model: [[https:// | * AMI Model: [[https:// | ||
- | * Schematic: {{: | + | * Schematic: {{: |
- | * Bill of Materials: {{: | + | * Bill of Materials: {{: |
- | * PCB Gerber Files: {{: | + | * PCB Gerber Files: {{: |
- | * PCB BRD File: {{: | + | * PCB BRD File: {{: |
- | * PCB Layout PDF: {{: | + | * PCB Layout PDF: {{: |
===== Software Needed ===== | ===== Software Needed ===== | ||
- | ===== Hardware Needed ===== | + | * [[: |
+ | * [[: | ||
+ | * [[adi> | ||
- | ===== AD9154 Evaluation Software ===== | + | <note important> |
- | The AD9154 Evaluation Board software runs on the ADI ACE graphical user interface (GUI). ACE is included on the Evaluation board CD. Registers on the AD9154 and AD9516 products are programmed by the ACE software via a USB cable connecting the user’s PC to the AD9154-FMC-EBZ XP2 connector. Software in the AD9154-FMC-EBZ PIC processor (XU1) provides the interface between the USB bus and the SPI busses of the AD9154 and AD9516. | + | |
- | ===== Hardware Setup ===== | + | |
- | | + | </note> |
- | <WRAP center> | + | |
- | {{: | + | |
- | | Figure 1. AD9154-FMC-EBZ Lab Block Diagram | + | |
- | {{: | + | |
- | | Figure 2. Top and Bottom view of AD9154-FMC-EBZ | + | |
- | </ | + | |
- | A spectrum analyzer should be connected to the EVB SMA connector J4. Connect SMA connectors J5, J14 and J17 of the EVB to an oscilloscope. The evaluation board connects to the ADS7 through the connector P1. The PC should be connected to the EVB using the mini-USB connector XP2. Figure 1 shows a block diagram of the set-up. | + | |
- | + | ||
- | === Clock input: === | + | |
- | A low phase noise high frequency clock source should be connected to the SMA connector J1. As seen in the schematic of AD9154-FMC-EBZ, | + | |
- | - direct DACCLK signal to the AD9154. The DACCLK is also routed to the AD9516' | + | |
- | - a reference clock to the AD9154' | + | |
- | + | ||
- | The AD9516 generates the bitrate/40 needed to establish a JESD204B link. If a JESD204B link needs to be established, | + | |
- | + | ||
- | If option #1 is needed, the J1 input is split between the AD9154 and the AD9516. | + | |
- | + | ||
- | If option #2 is needed, AD9154 may receive a reference clock either from the AD9516, as a divided down version of FIN, or directly from the J1 pin. In either case, the J1 input must be high enough to guarantee that the AD9516 can generate a bitrate/40 clock. | + | |
- | + | ||
- | + | ||
- | ===== Getting Started ===== | + | |
- | The PC software is included in the CD shipped with the EVB. The installation will include the software as well as all the AD9154 EVB files including schematic, board layout, datasheet, this quick start guide and other files. | + | |
- | ==== Initial Set-Up ==== | + | |
- | 1. Install the customer evaluation board software and support files, including DPGDownloader and ACE GUI on your PC. Follow the instructions in the installation wizard and use the default (recommended) installation settings. | + | |
- | 2. Plug the AD9154-FMC-EBZ into port FMC_1 of the ADS7 System. Use a USB cable to connect the EVB to your PC and connect the lab equipment to the EVB as shown in Figure 1. \\ \\ | + | |
- | 3. Connect the ADS7 unit to your PC via USB and turn on the ADS7. \\ \\ | + | |
- | 4. Connect SMA connector J5 to a spectrum analyzer, connect SMA connectors J17, J4 and J14 to an oscilloscope. | + | |
- | ==== Single Tone Demonstration ==== | + | |
- | === Single Tone Demo Lab Bench Configuration Procedure:=== | + | |
- | + | ||
- | These settings configure the AD9154 | + | |
- | + | ||
- | - Configure the hardware according to the hardware set-up instructions given in the Hardware Setup section above. Set the frequency of the DAC clock signal generator to 1500MHz, and the output level to 3dBm. The spectrum analyzer can be configured as shown in Figure 8 with a resolution bandwidth of 300kHz. Choose an Input Attenuation of 22dB. | + | |
- | + | ||
- | <WRAP center> | + | |
- | + | ||
- | {{:resources:eval: | + | |
- | | Figure 3. Initial DPG Downloader Panel | | + | |
- | </ | + | |
- | === Single Tone Demo Hardware and Software Start Up Procedure: | + | |
- | 1. Run DPG Downloader from Start->Analog Devices-> | + | |
- | + | ||
- | <WRAP center> | + | |
- | 2. Open ACE from Start->Analog Devices-> | + | |
- | 3. Press the AD9154 icon and populate the AD9154 initialization wizard as shown in figure 4b, JESD mode 0, Interpolation 2. Leave all other settings in their default state. Press rhe APPLY button. JESD204B PLL lock will turn green as shown in figure 4c. Press the AD9154 icon in the initialization wizard tab. The AD9154 block diagram view will appear populated as shown in figure 4d.\\ \\ | + | |
- | <WRAP center> | + | |
- | {{: | + | |
- | | Figure 4a. Initial ACE page for AD9154-FMC-EBZ | + | |
- | {{: | + | |
- | | Figure 4b. ACE AD9154 Initialization Wizard tab with selections made | | + | |
- | {{: | + | |
- | | Figure 4c. ACE AD9154 Initialization Wizard tab after pressing APPLY | | + | |
- | {{: | + | |
- | | Figure 4d. ACE AD9154 Block Diagram View after Initialization | + | |
- | </WRAP> | + | |
- | 4. In DPG Downloader Window Select Single Tone under the Add Generated Waveforms Tab. Set Data Rate: 750Mhz, Desired Frequency: 180Mhz, Amplitude: 0dbFS, Uncheck Unsigned Data, Check Generate Complex Data (I&Q) | + | |
- | + | ||
- | 5. Select JESD Mode: Mode 0, Select Subclass 0 | + | |
- | + | ||
- | 6. Populate the data playback selections for each DAC output as shown in Figure 5. | + | |
- | + | ||
- | 7. Click Download button and click Play button. The signals shown in figures 6 and 7 will appear on the DAC outputs (J17, J4, J5, and J14), Serial Line Rate will be 7.5Gbps. The green SYNC check mark indicates that the JESD204B link is up and running. | + | |
- | + | ||
- | + | ||
- | <WRAP center> | + | |
- | {{: | + | |
- | | Figure 5. AD9154-FMC-EBZ Fully Configured DPG Downloader Display | + | |
- | </ | + | |
- | + | ||
- | 8. Here’s what you will see on DAC0, DAC1, and DAC3 on the scope \\ \\ | + | |
- | + | ||
- | + | ||
- | + | ||
- | <WRAP center> | + | |
+ | ===== Hardware Needed ===== | ||
- | 9. Here is what you will see at the output of DAC2 on the Spectrum Analyzer. | + | * [[adi> |
+ | * USB-A to USB-Mini Cable | ||
+ | * [[: | ||
+ | * 12V 60W AC/DC Power Supply | ||
+ | * Power Cord | ||
+ | * USB-A to USB-B Cable | ||
+ | * PC with ACE and DPG Lite Software Applications | ||
+ | * Low Phase Noise High-Frequency Continuous Wave Generator | ||
+ | * Signal/Spectrum Analyzer | ||
+ | * 2 to 5 SMA Cables | ||
- | {{: | + | ===== Quick Start Guide ===== |
- | | Figure 6. DAC Output Spectrum Analyzer Display | + | - Attach AD9154-FMC-EBZ onto the FMC connector of ADS7-V2 controller board. Connect the evaluation board to PC via USB, the continuous waveform generator output to J1, one of the DAC outputs to a spectrum/ |
- | </ | + | - Set the frequency of the continuous waveform generator output to **1.5 GHz** and the output level to **+3 dBm**. Enable the output.< |
+ | - Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**, | ||
+ | - Open ACE. The board will automatically be recognized by the software as shown in Figure 3. Otherwise, install the plugin for AD9154 evaluation board by following the steps in this page: [[: | ||
+ | - In ACE, apply the configuration wizard settings enumerated below and shown in Figure 4. JESD204B PLL should lock and the indicator should turn green. | ||
+ | * **Links:** Single Link | ||
+ | * **JESD Mode:** 0 | ||
+ | * **Subclass1: | ||
+ | * **Interpolation: | ||
+ | * **DAC PLL:** False | ||
+ | * **FDAC:** 1.5 GHz <WRAP centeralign> | ||
+ | - In DPG Lite or DPG Downloader, configure single tone waveform generation. From the **Add Generator Waveforms** pulldown menu, select **Single Tone**. Apply the following settings: | ||
+ | * **Data Rate:** 750 MHz | ||
+ | * **Desired Frequency: | ||
+ | * **DAC Resolution: | ||
+ | * **Amplitude: | ||
+ | * **Unsigned Data:** unchecked | ||
+ | * **Generate Complex Data (I & Q):** checked | ||
+ | - In the ADS7-V2 panel in the DPG window, configure **Data Playback** by selecting tones for the DAC outputs from each dropdown menu. Set **JESD Mode** to Mode 0, **Links** to Single, and **Subclass** to 0. <WRAP centeralign> | ||
+ | - Press the download arrow ({{: | ||
- | {{: | ||
- | | |