This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:dpg:ad9152-fmc-ebz [12 Aug 2022 08:00] – [Software Needed] Shine Cabatan | resources:eval:dpg:ad9152-fmc-ebz [11 Oct 2022 14:05] (current) – [Software Needed] Shine Cabatan | ||
---|---|---|---|
Line 37: | Line 37: | ||
<note important> | <note important> | ||
- | * If using ADS8-V1EBZ, install {{https:// | ||
* Do not install ACE on a computer with DAC Software Suite. | * Do not install ACE on a computer with DAC Software Suite. | ||
* **Known Issue:** ACE may fail to detect HS-DAC boards, details [[resources: | * **Known Issue:** ACE may fail to detect HS-DAC boards, details [[resources: | ||
Line 57: | Line 56: | ||
===== Quick Start Guide ===== | ===== Quick Start Guide ===== | ||
- | - Attach AD9152-FMC-EBZ onto the FMC connector of ADS7-V2 or ADS8-V1 controller board. Connect the evaluation board to PC via USB, the continuous waveform generator output to J1, and one of the DAC outputs (J4 or J17) to a signal/ | + | - Attach AD9152-FMC-EBZ onto the FMC connector of ADS7-V2 or ADS8-V1 controller board. Connect the evaluation board to PC via USB, the continuous waveform generator output to J1, and one of the DAC outputs (J4 or J17) to a signal/ |
- Set the frequency of the continuous waveform generator output to **1.5 GHz** and the output level to **+3 dBm**. Enable the output. <WRAP centeralign> | - Set the frequency of the continuous waveform generator output to **1.5 GHz** and the output level to **+3 dBm**. Enable the output. <WRAP centeralign> | ||
- Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**, | - Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**, |