This is an old revision of the document!
This user guide describes both the hardware and software setup needed to acquire data capture from AD9152-FMC-EBZ evaluation board to characterize AD9152 16-bit 2.25Gsps dual JESD204B signal processing RF Digital to Analog Converter.
The AD9152-FMC-EBZ is an FMC mezzanine card and connects to an ADS7-V2 or ADS8-V1 data pattern generator system. The ADS7-V2/ADS8-V1 automatically formats the data and sends it to the AD9152-FMC-EBZ via its JESD204B lanes. The AD9152-FMC-EBZ is an FMC mezzanine card. +12V, +3.3V, and VADJ power supply rails are provided by the ADS7-V2/ADS8-V1 system via the FMC connector P1. A clock distribution chip AD9516 is included on this EVB as a clock fan-out and frequency divider for the DACCLK, JESD204B SYSREF signals, and a GBTCLK clock used by the ADS7-V2/ADS8-V1. There is also an FMC standard I2C bus that is used by the ADS7-V2/ADS8-V1 to identify the AD9152-FMC-EBZ. This I2C interface is implemented in software in the AD9152-FMC-EBZ PIC processor (XU1). All ADS7-V2/ADS8-V1 to/from AD9152-FMC-EBZ interface signals are connected via the FMC connector P1.
A low phase noise high frequency clock source should be connected to the SMA connector J1, This is the DACCLK input. The spectrum analyzer should be connected to the SMA connector,J4 or J17. The evaluation board connects to the ADS7 through the connectors P3. The PC should be connected to the EVB using the mini-USB connector XP2 after installation of the Evaluation Board software. Figure 1 shows the block diagram of the set-up.
1. Install ACE software or SPIPro software and support files on your PC. Follow the instructions in the installation wizard and use the default (recommended) installation settings.
2. Plug the AD9152-FMC-EBZ into port FMC_1 of the ADS7 System. Use a USB cable to connect the EVB to your PC and connect the lab equipment to the EVB as shown in Figure 1.
3. Connect the ADS7 unit to your PC via USB and turn on the ADS7.
These settings configure the AD9152 to output a sine wave using the ADS7 and allow the
user to view the single-tone performance at the DAC output, under the condition: Fdata = 375MHz, 4X interpolation, Fout = 100MHz.
Following settings configure the AD9152 to output a 100Mhz (-10dbFS) sine wave using the ADS7 on both 2 of AD9152 DACs.
- Configure the hardware according to the hardware set-up instructions given in the Hardware Setup section above. Set the frequency of the DAC clock signal generator to 1500MHz, and the output level to 3dBm. The spectrum analyzer can be configured as shown in Figure 6 with a resolution bandwidth of 30kHz. Choose an Input Attenuation of 10dB.
1. Open DPG Downloader Lite. It will say AD9152 as shown in Figure 3.
2. Open ACE from the start window. It can be found by following the file path to the program or by searching in the windows search bar for “ACE.” The icon indicates the ACE software.
3. If the board is connected properly, ACE will detect it and display it on the Start page under “Attached Hardware.” Double click this board.
4. Ensure that the button is green in the subsystem image under the “System” tab. If not, click it, select the AD9152, and click “Acquire.” Double click on the subsystem image.
5. To the left of the board diagram, click “Modify” under “Initial Configuration Summary” to edit the DAC and PLL setup of the board. In some cases, the “Initial Configuration” page will already be shown.
6. Alter the inputs to match the figure below. Click “Apply.”
7. Double click on the dark blue AD9152 on the board diagram. Ensure that the settings of the AD9152 match with the chip diagram in the figure below and click “Apply Changes.” The “Poll Devices” button and JESD PLL Locked should both be enabled. If neither are enabled, click “Read All” or reset the board, reset the chip, and reapply the settings for the board and chip. For more information about ACE, see the “ACE Software Features” section.
8. On the DPGDownloader panel, select Single Tone under the Add Generated Waveforms Tab. Set Data Rate: 375Mhz, Desired Frequency: 100Mhz, Amplitude: -10dbFS, Uncheck Unsigned Data, Check Generate Complex Data (I and Q).
9. Click Download () and Play () in the DPG Downloader screen. The spectrum in Figure 10 will appear on all 2 DAC outputs (J17, J4, ), Serial Line Rate will be 3.75Gsps.
10.Here is what you will see at the output of DAC0 on the Spectrum Analyzer.
1. On your lab computer, open the SPIPro application (Start > All Programs > Analog Devices > AD9152 > SPIPro). You will see the GUI shown in Figure 12 come up. Run DPG Downloader Lite. It will say AD9152 as shown in Figure 11.
2. Open SPIPro. It will show AD9152-FMC-EBZ in the upper left hand corner.
3. Select single link, JESD mode 4, Interpolation 4. Press ‘Configure DAC and Clock’ button. JESD204B PLL lock will turn green.
4. Select Single Tone under the Add Generated Waveforms Tab. Set Data Rate: 375Mhz, Desired Frequency: 100Mhz, Amplitude: -10dbFS, Uncheck Unsigned Data, Check Generate Complex Data (I and Q).
5. Click Download () and Play () in the DPG Downloader screen. The spectrum in figure 6 will appear on all 2 DAC outputs (J17, J4, ), Serial Line Rate will be 3.75Gsps.
6. Here is what you will see at the output of DAC0 on the Spectrum Analyzer.