This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:dpg:ad9142a-m5372-ebz [15 Jun 2017 19:49] Bailey Meyer |
resources:eval:dpg:ad9142a-m5372-ebz [16 Jun 2017 16:02] Bailey Meyer |
||
---|---|---|---|
Line 34: | Line 34: | ||
If the board is connected properly, ACE will detect it and display it on the Start page under //Attached Hardware//. Double click this board. | If the board is connected properly, ACE will detect it and display it on the Start page under //Attached Hardware//. Double click this board. | ||
- | {{ :resources:eval:user-guides:ad9129_detected.png }} | + | {{ :resources:eval:user-guides:ad9142a_detected_new.png }} |
<WRAP clear> | <WRAP clear> | ||
</WRAP> | </WRAP> | ||
- | <WRAP centeralign> Figure 3. Detected AD9129 detected in ACE. The AD9142A will be displayed in the same way. </WRAP> | + | <WRAP centeralign> Figure 3. Detected AD9142A-M537x in ACE. </WRAP> |
Ensure that the {{:resources:eval:user-guides:connection_icon.png}} button in lower left corner of the subsystem image (located under the "System" tab) is green, meaning the board is connected. If not, click it, select the AD739A, and click "Acquire." Double click on the subsystem image to reach the board block diagram. | Ensure that the {{:resources:eval:user-guides:connection_icon.png}} button in lower left corner of the subsystem image (located under the "System" tab) is green, meaning the board is connected. If not, click it, select the AD739A, and click "Acquire." Double click on the subsystem image to reach the board block diagram. | ||
- | {{ :resources:eval:user-guides:ad9129_system.png }} | + | {{ :resources:eval:user-guides:ad9142a_system_new.png }} |
<WRAP clear> | <WRAP clear> | ||
</WRAP> | </WRAP> | ||
- | <WRAP centeralign> Figure 4. The AD9129 system. The AD9142A will be displayed in the same way. </WRAP> | + | <WRAP centeralign> Figure 4. The AD9142A-M537x system. </WRAP> |
2. Configure the hardware according to the hardware set-up instructions given in the Hardware Setup section above. Set the frequency of the DAC clock signal generator to 1400MHz, and the output level to 6dBm. The spectrum analyzer can be configured with Center Frequency = 2050 MHz, Span = 200 MHz, and Resolution Bandwidth of 30 kHz. Choose Input Attenuation to be 24dB. This can be adjusted later if indications are that the analyzer is causing degradations. \\ \\ | 2. Configure the hardware according to the hardware set-up instructions given in the Hardware Setup section above. Set the frequency of the DAC clock signal generator to 1400MHz, and the output level to 6dBm. The spectrum analyzer can be configured with Center Frequency = 2050 MHz, Span = 200 MHz, and Resolution Bandwidth of 30 kHz. Choose Input Attenuation to be 24dB. This can be adjusted later if indications are that the analyzer is causing degradations. \\ \\ |