This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:dpg:ad9142-m5375-ebz [03 Dec 2012 09:17] – 2nd edit_whole Patrick Xuan | resources:eval:dpg:ad9142-m5375-ebz [04 Dec 2012 08:16] (current) – [Single-Tone Test] Patrick Xuan | ||
---|---|---|---|
Line 18: | Line 18: | ||
<WRAP center> | <WRAP center> | ||
- | | {{ : | + | | {{ : |
| Figure 1. Block diagram of the AD9142 lab bench set-up | | Figure 1. Block diagram of the AD9142 lab bench set-up | ||
</ | </ | ||
Line 67: | Line 67: | ||
</ | </ | ||
- | 4. The current on the 5V supply should read about 1220mA. \\ | + | 4. The current on the 5V supply should read about 1190mA. \\ |
<WRAP center> | <WRAP center> | ||
- | | {{ : | + | | {{ : |
| Figure 7 AD9142-M5375 Eval Board output Spectrum | | Figure 7 AD9142-M5375 Eval Board output Spectrum | ||
</ | </ | ||
Line 100: | Line 100: | ||
<WRAP center> | <WRAP center> | ||
^ Output Viewed ^ SMA Connector ^ Jumper Configurations^ | ^ Output Viewed ^ SMA Connector ^ Jumper Configurations^ | ||
- | | I DAC Output | + | | I DAC Output |
- | | Q DAC Output | + | | Q DAC Output |
| ADL5372 RF Output | | ADL5372 RF Output | ||
</ | </ |