This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:dpg:ad9142-m5375-ebz [03 Dec 2012 08:35] – created Patrick Xuan | resources:eval:dpg:ad9142-m5375-ebz [04 Dec 2012 08:16] (current) – [Single-Tone Test] Patrick Xuan | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AD9142-M5372-EBZ Evaluation Board Quick Start Guide ====== | + | ====== AD9142-M5375-EBZ Evaluation Board Quick Start Guide ====== |
- | ===== Getting Started with the AD9142-M5372-EBZ Evaluation Board and Software ===== | + | ===== Getting Started with the AD9142-M5375-EBZ Evaluation Board and Software ===== |
==== What's in the Box ==== | ==== What's in the Box ==== | ||
- | * AD9142-M5372-EBZ Evaluation Board | + | * AD9142-M5375-EBZ Evaluation Board |
* Evaluation Board CD | * Evaluation Board CD | ||
* Mini-USB Cable | * Mini-USB Cable | ||
Line 11: | Line 11: | ||
* Data Pattern Generator Series 2 (DPG2) | * Data Pattern Generator Series 2 (DPG2) | ||
== Introduction ===== | == Introduction ===== | ||
- | The AD9142-M5372-EBZ connects to a DPG2 for quick evaluation of the AD9142, a high-speed, signal processing Digital to Analog Converter. The DPG2 automatically formats the data and sends it to the AD9142-M5372-EBZ, simplifying evaluation of the device. The Evaluation Board (EVB) runs from a +5V supply. A clock distribution chip AD9516 is included on this EVB as a clock fan-out and frequency divider for the DACCLK, REFCLK and DPG2 input clock. Also included is a quadrature modulator | + | The AD9142-M5375-EBZ connects to a DPG2 for quick evaluation of the AD9142, a high-speed, signal processing Digital to Analog Converter. The DPG2 automatically formats the data and sends it to the AD9142-M5375-EBZ, simplifying evaluation of the device. The Evaluation Board (EVB) runs from a +5V supply. A clock distribution chip AD9516 is included on this EVB as a clock fan-out and frequency divider for the DACCLK, REFCLK and DPG2 input clock. Also included is a quadrature modulator |
===== AD9142 Evaluation Software ===== | ===== AD9142 Evaluation Software ===== | ||
The AD9142 Evaluation Board software has an easy-to-use graphical user interface (GUI). It is included on the Evaluation Board CD, or can be downloaded from the DPG website at http:// | The AD9142 Evaluation Board software has an easy-to-use graphical user interface (GUI). It is included on the Evaluation Board CD, or can be downloaded from the DPG website at http:// | ||
Line 18: | Line 18: | ||
<WRAP center> | <WRAP center> | ||
- | | {{ : | + | | {{ : |
- | | Figure 1. Block diagram of the AD9142 lab bench set-up | + | | Figure 1. Block diagram of the AD9142 lab bench set-up |
</ | </ | ||
===== Getting Started ===== | ===== Getting Started ===== | ||
Line 67: | Line 67: | ||
</ | </ | ||
- | 4. The current on the 5V supply should read about 1220mA. \\ | + | 4. The current on the 5V supply should read about 1190mA. \\ |
<WRAP center> | <WRAP center> | ||
- | | {{ : | + | | {{ : |
- | | Figure 7 AD9142-M5372 Eval Board output Spectrum | + | | Figure 7 AD9142-M5375 Eval Board output Spectrum |
</ | </ | ||
===== SPI SOFTWARE ===== | ===== SPI SOFTWARE ===== | ||
Line 100: | Line 100: | ||
<WRAP center> | <WRAP center> | ||
^ Output Viewed ^ SMA Connector ^ Jumper Configurations^ | ^ Output Viewed ^ SMA Connector ^ Jumper Configurations^ | ||
- | | I DAC Output | + | | I DAC Output |
- | | Q DAC Output | + | | Q DAC Output |
| ADL5372 RF Output | | ADL5372 RF Output | ||
</ | </ | ||
Note: When viewing the modulator output, a local oscillator (LO) must be connected to J15 (”LO_IN”) to properly modulate the signals. | Note: When viewing the modulator output, a local oscillator (LO) must be connected to J15 (”LO_IN”) to properly modulate the signals. | ||
+ |