Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:dpg:ad9136-fmc-ebz [12 Aug 2022 12:03]
Shine Cabatan [Quick Start Guide]
resources:eval:dpg:ad9136-fmc-ebz [11 Oct 2022 14:05]
Shine Cabatan [Software Needed]
Line 40: Line 40:
  
 <note important>​ <note important>​
-  * If using AD9135-FMC-EBZ with ADS8-V1EBZ, install {{https://​swdownloads.analog.com/​ACE/​ACEInstall_1.25.3217.1405.exe|ACE v1.25.}} 
   * Do not install ACE on a computer with DAC Software Suite.   * Do not install ACE on a computer with DAC Software Suite.
   * **Known Issue:** ACE may fail to detect HS-DAC boards, details [[resources:​tools-software:​ace:​knownissues#​high-speed_dac_eval_boards_are_not_discovered|here]].   * **Known Issue:** ACE may fail to detect HS-DAC boards, details [[resources:​tools-software:​ace:​knownissues#​high-speed_dac_eval_boards_are_not_discovered|here]].
Line 63: Line 62:
   - Set the frequency of the continuous waveform generator output to **2.0 GHz** and the output level to **+3 dBm**. Enable the output.<​WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9136-fmc-ebz_dpg_board_detect.png?​600 |}}//Figure 3. ADS7-V2 and AD9136 detected in DPG Software//</​WRAP>​   - Set the frequency of the continuous waveform generator output to **2.0 GHz** and the output level to **+3 dBm**. Enable the output.<​WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9136-fmc-ebz_dpg_board_detect.png?​600 |}}//Figure 3. ADS7-V2 and AD9136 detected in DPG Software//</​WRAP>​
   - Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**,​ respectively. <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9136-fmc-ebz_ace_board_detect.png?​600 |}}//Figure 4. AD9136-FMC-EBZ detected in ACE//</​WRAP>​   - Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**,​ respectively. <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9136-fmc-ebz_ace_board_detect.png?​600 |}}//Figure 4. AD9136-FMC-EBZ detected in ACE//</​WRAP>​
-  - Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9135/​AD9136 evaluation board by following the steps in this page: [[:​resources:​tools-software:​ace:​userguide:​quickstart|Quickstart - ACE Quickstart and Plug-in Installation]]. <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9136-fmc-ebz_ace_configuration_wizard.png?​600 |}}//Figure 5. ACE Initial Configuration Wizard//</​WRAP><​WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9136-fmc-ebz_ace_chipview.png?​600 |}}//Figure 6. ACE AD9152 ​Chipview Tab//</​WRAP>​+  - Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9135/​AD9136 evaluation board by following the steps in this page: [[:​resources:​tools-software:​ace:​userguide:​quickstart|Quickstart - ACE Quickstart and Plug-in Installation]]. <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9136-fmc-ebz_ace_configuration_wizard.png?​600 |}}//Figure 5. ACE Initial Configuration Wizard//</​WRAP><​WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9136-fmc-ebz_ace_chipview.png?​600 |}}//Figure 6. ACE AD9136 ​Chipview Tab//</​WRAP>​
   - In ACE, apply the configuration wizard settings enumerated below and shown in Figure 5. JESD204B PLL should lock and the indicator should turn green.   - In ACE, apply the configuration wizard settings enumerated below and shown in Figure 5. JESD204B PLL should lock and the indicator should turn green.
        * **Links:** Dual Link        * **Links:** Dual Link
Line 70: Line 69:
        * **Interpolation:​** 1        * **Interpolation:​** 1
        * **DAC PLL:** False        * **DAC PLL:** False
-       * **FDAC:** 2 GHz+       * **FDAC:** 2 GHz<WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9136-fmc-ebz_dpg_output_generation.png?​600 |}}//Figure 7. Single Tone and ADS7-V2 Configuration Panels in DPG//</​WRAP>​
   - In DPG Lite or DPG Downloader, configure generation of two single tone waveforms. From the **Add Generator Waveforms** pulldown menu, select **Single Tone**. Do this two times then configure the panels as follows:   - In DPG Lite or DPG Downloader, configure generation of two single tone waveforms. From the **Add Generator Waveforms** pulldown menu, select **Single Tone**. Do this two times then configure the panels as follows:
        * **Data Rate** = 2 GHz, **Amplitude** = -1dBFS, **Unsigned Data** is unchecked for both panels.        * **Data Rate** = 2 GHz, **Amplitude** = -1dBFS, **Unsigned Data** is unchecked for both panels.
        * **Desired Frequency = 112 MHz** in one panel while **Desired Frequency = 221 MHz** in the other.        * **Desired Frequency = 112 MHz** in one panel while **Desired Frequency = 221 MHz** in the other.
        * If using AD9135, set **DAC Resolution** to **11 bits**. Otherwise, leave as is (16 bits).        * If using AD9135, set **DAC Resolution** to **11 bits**. Otherwise, leave as is (16 bits).
-  - In the ADS7-V2 or ADS8-V1 panel in the DPG window, configure **Data Playback** by selecting tone2 for DAC0 and tone1 for DAC1. Set **JESD Mode** to Mode 8, **Links** to Dual, and **Subclass** to 1. <WRAP centeralign>​ {{ :​resources:​eval:​dpg:​ad9136:​ad9136-35_dac0_sa_output.png?​600 | }}//​Figure ​7. DAC0 Output Spectrum Analyzer Display// </​WRAP>​ <WRAP centeralign>​ {{ :​resources:​eval:​dpg:​ad9136:​ad9136-35_dac1_scope_output.png?​600 | }}//​Figure ​8. DAC1 Output Scope Display// </​WRAP>​ +  - In the ADS7-V2 or ADS8-V1 panel in the DPG window, configure **Data Playback** by selecting tone2 for DAC0 and tone1 for DAC1. Set **JESD Mode** to Mode 8, **Links** to Dual, and **Subclass** to 1. <WRAP centeralign>​ {{ :​resources:​eval:​dpg:​ad9136:​ad9136-35_dac0_sa_output.png?​600 | }}//​Figure ​8. DAC0 Output Spectrum Analyzer Display// </​WRAP>​ <WRAP centeralign>​ {{ :​resources:​eval:​dpg:​ad9136:​ad9136-35_dac1_scope_output.png?​600 | }}//​Figure ​9. DAC1 Output Scope Display// </​WRAP>​ 
-  - Press the download arrow ({{:​resources:​eval:​dpg:​9154_down_arrow.png}}) then the play button ({{:​resources:​eval:​dpg:​9154_right_green_arrow.png}}). **Serial Line Rate** should appear as 10 Gbps and **Sync Status** should have two check marks. Refer to FFT plot of the DAC0 output in Figure ​and the oscilloscope capture of DAC1 output in Figure ​8.+  - Press the download arrow ({{:​resources:​eval:​dpg:​9154_down_arrow.png}}) then the play button ({{:​resources:​eval:​dpg:​9154_right_green_arrow.png}}). **Serial Line Rate** should appear as 10 Gbps and **Sync Status** should have two check marks. Refer to FFT plot of the DAC0 output in Figure ​and the oscilloscope capture of DAC1 output in Figure ​9.
resources/eval/dpg/ad9136-fmc-ebz.txt · Last modified: 11 Oct 2022 14:05 by Shine Cabatan