Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:dpg:ad9122-ebz [23 Apr 2018 19:05]
Annette Hurman [Software Installation]
resources:eval:dpg:ad9122-ebz [09 May 2018 17:22]
Annette Hurman [Generating a Test Vector with ACE]
Line 27: Line 27:
 {{ :​resources:​eval:​dpg:​pics-001.jpg?​400 |}} {{ :​resources:​eval:​dpg:​pics-001.jpg?​400 |}}
 Figure 2. DPG2 and AD9122 Evaluation Board  Figure 2. DPG2 and AD9122 Evaluation Board 
-{{ :resources:eval:dpg:​sdph1-ad9747-1.png?300 |}}+{{ :resources/eval/dpg/​ad9121_25_visio_diag.jpg?300 |}}
 Figure 3. SDP-H1 and AD9122 Evaluation Board Bench set-up Figure 3. SDP-H1 and AD9122 Evaluation Board Bench set-up
 {{ :​resources:​eval:​dpg:​sdph1-ad9747-2.png?​300 |}} {{ :​resources:​eval:​dpg:​sdph1-ad9747-2.png?​300 |}}
Line 48: Line 48:
 ==== Generating a Test Vector with ACE ==== ==== Generating a Test Vector with ACE ====
 1. Power up the DPG and connect the USB cable to the PC.\\ \\ 1. Power up the DPG and connect the USB cable to the PC.\\ \\
-2. Next, run the DPGDownloader Software. To launch DPGDownloader,,​ click Start > Programs > Analog Devices > DPG > DPGDownloader. If the AD9122 evaluation board has been recognized by the PC, AD9122 should be populated in the Evaluation Board field in the Hardware Config panel.\\ \\+2. Next, run the DPGDownloader Software. To launch DPGDownloader,,​ click Start > Programs > Analog Devices > DPG > DPGDownloader. If the AD9122/21 evaluation board has been recognized by the PC, AD9122/21 should be populated in the Evaluation Board field in the Hardware Config panel.\\ \\
 3. Generate a sine wave by pulling down the “Add Generated Waveform” menu and choosing “Single Tone”. Fill in the form as shown below (Sample Rate = 250MHz, Desired Frequency = 29 MHz, etc.). Note that the Sample Rate should match the input sample rate and not the DAC update rate.\\ \\ 3. Generate a sine wave by pulling down the “Add Generated Waveform” menu and choosing “Single Tone”. Fill in the form as shown below (Sample Rate = 250MHz, Desired Frequency = 29 MHz, etc.). Note that the Sample Rate should match the input sample rate and not the DAC update rate.\\ \\
 {{ :​resources:​eval:​dpg:​dpgdownloader9122.png?​640 }} \\ {{ :​resources:​eval:​dpg:​dpgdownloader9122.png?​640 }} \\
resources/eval/dpg/ad9122-ebz.txt · Last modified: 09 May 2018 17:22 by Annette Hurman