Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Last revision Both sides next revision
resources:eval:dpg:ad9122-ebz [14 Sep 2017 15:17]
Michele Viani [Software Installation]
resources:eval:dpg:ad9122-ebz [07 May 2018 18:46]
Annette Hurman [Hardware Setup (DAC OUTPUT)]
Line 1: Line 1:
-====== AD9122 Evaluation Board Quick Start Guide ====== +====== ​AD9121/AD9122 Evaluation Board Quick Start Guide ====== 
-===== Getting Started with the AD9122 Evaluation Board =====+===== Getting Started with the AD9121/AD9122 Evaluation Board =====
 ==== What's in the Box ==== ==== What's in the Box ====
   * AD9122-M5375-EBZ or AD9122-M5372-EBZ Evaluation Board    * AD9122-M5375-EBZ or AD9122-M5372-EBZ Evaluation Board 
   * Mini-USB Cable    * Mini-USB Cable 
-  * AD9122 Evaluation Board CD+  * AD9121/AD9122 Evaluation Board CD
 ==== Recommended Equipment ==== ==== Recommended Equipment ====
-  * Digital Pattern Generator Series 2 or 3 (DPG): ADI HSC-DAC-DPG-BZ ​+  * Digital Pattern Generator Series 2 or 3 (DPG): ADI HSC-DAC-DPG-BZ ​OR System Demonstration Platform( SDP-H1) and FMC to High-Speed DAC Evaluation Board Adaptor(AD-DAC-FMC-ADP)
   * +5Vdc Power Supply Ex: Agilent E3630A   * +5Vdc Power Supply Ex: Agilent E3630A
   * DAC Clock Source Ex: Rohde Schwarz SML 02    * DAC Clock Source Ex: Rohde Schwarz SML 02 
Line 13: Line 13:
   * PC: Windows PC with 2 or more USB ports   * PC: Windows PC with 2 or more USB ports
 ==== Introduction ==== ==== Introduction ====
-The AD9122 Evaluation Board connects to the Analog Devices Digital Pattern Generator (DPG) to allow for quick evaluation of the AD9122. The DPG allows the user to create many types of digital vectors and transmit these at speed to the AD9122 in any of the AD9122 operating modes. The AD9122 evaluation board is configured over USB with accompanying PC software.+The AD9121/AD9122 Evaluation Board connects to the Analog Devices Digital Pattern Generator (DPG) or System Demonstration Platform (SDP-H1, PN: EVAL-SDP-CH1Z) to allow for quick evaluation of the AD9121/AD9122. The DPG or SDP-H1 ​allows the user to create many types of digital vectors and transmit these at speed to the AD9122 in any of the AD9121/AD9122 operating modes. The AD9121/AD9122 evaluation board is configured over USB with accompanying PC software.
 ==== Software Installation ==== ==== Software Installation ====
-The DAC Software Suite plus AD9122 Update should be installed on the PC prior connecting the hardware to the PC. The DAC Software Suite is included on the Evaluation Board CD, or can be downloaded from the DPG web site at https://​wiki.analog.com/​resources/​eval/​dpg/​dacsoftwaresuite. This will install DPGDownloader (for loading vectors into the DPG2) and the AD9122 SPI Controller application. However, ACE, a newer evaluation software from ADI, is the preferred evaluation software over the legacy SPI control graphical user interface (GUI). ACE can be downloaded from the ACE website at www.analog.com/​ace. The ACE plug-in for the evaluation board, which is also required, is available for download on the AD9122 eval webpage in the software section at http://​www.analog.com/​en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​EVAL-AD9122.html#​eb-relatedsoftware.  +The DAC Software Suite plus AD9121/AD9122 Update should be installed on the PC prior to connecting the hardware to the PC. The DAC Software Suite is included on the Evaluation Board CD, or can be downloaded from the DPG web site at https://​wiki.analog.com/​resources/​eval/​dpg/​dacsoftwaresuite. This will install DPGDownloader (for loading vectors into the DPG2) and the AD9121/AD9122 SPI Controller application. However, ACE, a newer evaluation software from ADI, is the preferred evaluation software over the legacy SPI control graphical user interface (GUI). ACE can be downloaded from the ACE website at www.analog.com/​ace. The ACE plug-in for the evaluation board, which is also required, is available for download on the AD9121/AD9122 eval webpage in the software section at http://​www.analog.com/​en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​EVAL-AD9122.html#​eb-relatedsoftware.  
-==== Hardware Setup ==== +==== Hardware Setup (DAC OUTPUT) ​==== 
-Once DPGDownloader is installed, the hardware can be connected as shown below. A single 5V power supply powers the evaluation board. The power supply should be able to source up to 2A to cover all of the board’s operating conditions. A low jitter clock source (< 0.5psec RMS) should be used for the DACCLK. A sinusoidal clock output level of 0 to 4dBm is optimal. By default, the DAC outputs are connected to SMA connectors for evaluation. Both DAC outputs are available. Later in document, the modifications for observing the modulator output and different clocking options will be shown. The evaluation board plugs directly into the DPG. The PC connects to both the DPG and the evaluation board through USB cables. +Once the DPGDownloader ​software ​is installed, the hardware can be connected as shown below. A single 5V power supply powers the evaluation board. The power supply should be able to source up to 2A to cover all of the board’s operating conditions. A low jitter clock source (< 0.5psec RMS) should be used for the DACCLK. A sinusoidal clock output level of 0 to 4dBm is optimal. By default, the DAC outputs are connected to SMA connectors for evaluation. Both DAC outputs are available. Later in the document, the modifications for observing the modulator output and different clocking options will be shown. 
-Equipment ​        ^ Connects to AD9122 Eval Board       ^ +  * The evaluation board plugs directly into the DPG2 or DPG3. 
-Power Supply ​     ​| ​P5 (+5V), P6 (GND)| +The PC connects to both the DPG2 and the evaluation board through USB cables ​as showing in Figure 1 and Figure 2  
-Signal Source ​    | J1 (CLKIN), Set source to 500MHz, 2dBm output ​| +  * The evaluation boards plugs into the AD-DAC-FMC-ADP adapter board that plugs into the SDP-H1
-PC USB Cable      ​| ​XP2 | +The PC connects to both the SDP-H1 and the evaluation board through USB cables as shown in Figure 3 and Figure 4. 
-Spectrum Analyzer ​J3 (DAC1_P) or J8 (DAC2_P)| + 
-DPG2              ​| ​P1 and P2 | +{{ :​resources:​eval:​dpg:​pics-000.jpg?​400 |}} 
-{{:​resources:​eval:​dpg:​pics-000.jpg?​400|}}{{ :​resources:​eval:​dpg:​pics-001.jpg?​400|}}+Figure 1. DPG2 and AD9122 Evaluation Board Bench set-up 
 +{{ :​resources:​eval:​dpg:​pics-001.jpg?​400 |}} 
 +Figure 2. DPG2 and AD9122 Evaluation Board  
 +{{ :​resources/​eval/​dpg/​ad9121_25_visio_diag.jpg?​300 |}} 
 +Figure 3. SDP-H1 and AD9122 Evaluation Board Bench set-up 
 +{{ :​resources:​eval:​dpg:​sdph1-ad9747-2.png?​300 |}} 
 +Figure 4. SDP-H1 and AD9122 Evaluation Board  
 + 
 +=====  BASIC HARDWARE SETUP ===== 
 +Connect the equipment to the AD9122 evaluation board per the following table: 
 +  * Equipment Connects to AD9122 Eval Board 
 +  ​* ​Power Supply P5(+5V),​ P6(GND) 
 +  ​* ​Signal Source ​ J1(CLOCK IN), Set source to 500MHz, 2dBm output 
 +  ​* ​PC USB Cable  XP2 
 +  ​* ​Spectrum Analyzer J3 (DAC1_P) or J8 (DAC2_P) 
 +  ​* ​DPG2 P1 and P2 
 +  * SDP-H1 J4(FMC connector) 
  
 ===== Getting Started ===== ===== Getting Started =====
-It is suggested that the basic set-up ​is verified before making any modifications to the evaluation board.+It is suggested that the basic set-up ​be verified before making any modifications to the evaluation board.
  
 ==== Generating a Test Vector with ACE ==== ==== Generating a Test Vector with ACE ====
Line 52: Line 69:
  
 ==== Generating a Test Vector with the SPI Controller ==== ==== Generating a Test Vector with the SPI Controller ====
-Launch the AD9122 SPI GUI by clicking the AD9122 SPI button.+Launch the AD9122 SPI GUI by clicking the AD9122 SPI button.\\ \\
 1. Power up the DPG and connect the USB cable to the PC.\\ \\ 1. Power up the DPG and connect the USB cable to the PC.\\ \\
 2. Next, run the DPGDownloader Software. To launch DPGDownloader,,​ click Start > Programs > Analog Devices > DPG > DPGDownloader. If the AD9122 evaluation board has been recognized by the PC, AD9122 should be populated in the Evaluation Board field in the Hardware Config panel.\\ \\ 2. Next, run the DPGDownloader Software. To launch DPGDownloader,,​ click Start > Programs > Analog Devices > DPG > DPGDownloader. If the AD9122 evaluation board has been recognized by the PC, AD9122 should be populated in the Evaluation Board field in the Hardware Config panel.\\ \\
resources/eval/dpg/ad9122-ebz.txt · Last modified: 09 May 2018 17:22 by Annette Hurman