resources:eval:dpg:ad9119-mix-ebz [12 Oct 2012 20:34]
Dan Fague [Hardware Setup]
resources:eval:dpg:ad9119-mix-ebz [02 Nov 2012 20:38] (current)
Dan Fague [Mix-Mode Operation]
Line 1: Line 1:
-~~UNDERCONSTRUCTION~~ 
 ====== AD9119-MIX-EBZ Evaluation Board Quick Start Guide ====== ====== AD9119-MIX-EBZ Evaluation Board Quick Start Guide ======
 ===== Getting Started with the AD9119 Mix-mode(tm) Evaluation Board and Software ===== ===== Getting Started with the AD9119 Mix-mode(tm) Evaluation Board and Software =====
Line 19: Line 18:
  
  
-<​WRAP ​col2 50%>+<​WRAP ​column 40%>
 {{:​resources:​eval:​dpg:​ad9129:​bench_setup_9119_evb.png?​350 |}}  {{:​resources:​eval:​dpg:​ad9129:​bench_setup_9119_evb.png?​350 |}} 
 </​WRAP>​ </​WRAP>​
-<​WRAP ​right 50%>+<​WRAP ​column 55%>
 {{:​resources:​eval:​dpg:​ad9129:​figure2_9129-MIX-EBZ.png?​400 |}}  {{:​resources:​eval:​dpg:​ad9129:​figure2_9129-MIX-EBZ.png?​400 |}} 
 </​WRAP>​ </​WRAP>​
 <WRAP clear> <WRAP clear>
 </​WRAP>​ </​WRAP>​
-<​WRAP ​col2 50%>+<​WRAP ​column 40%>
 Figure 1 - Block diagram of the AD9119 lab bench set-up Figure 1 - Block diagram of the AD9119 lab bench set-up
 </​WRAP>​ </​WRAP>​
-<​WRAP ​right 50%>+<​WRAP ​column 55%>
 Figure 2 - Top view of AD9119-MIX-EBZ Evaluation Board (uses the AD9129 EVB) Figure 2 - Top view of AD9119-MIX-EBZ Evaluation Board (uses the AD9129 EVB)
 </​WRAP>​ </​WRAP>​
Line 119: Line 118:
 When using mix-mode and targeting a signal to the second Nyquist zone, it is important to remember that the center frequency chosen in the DPG window is the offset from the DACCLK sample frequency, not 0 Hz. For example, to place the carrier at 1982.5 MHz with a 2.4576 GHz DACCLK as in Figure 12, program the DPG Downloader center frequency to 475 MHz and enable mix-mode. Figure 12 shows the IMD performance of several different DAC output currents and the loss in output power expected with lower currents. ​ When using mix-mode and targeting a signal to the second Nyquist zone, it is important to remember that the center frequency chosen in the DPG window is the offset from the DACCLK sample frequency, not 0 Hz. For example, to place the carrier at 1982.5 MHz with a 2.4576 GHz DACCLK as in Figure 12, program the DPG Downloader center frequency to 475 MHz and enable mix-mode. Figure 12 shows the IMD performance of several different DAC output currents and the loss in output power expected with lower currents. ​
  
-<​WRAP ​col2 50%> {{:​resources:​eval:​dpg:​ad9129:​figure12b_9129-MIX-EBZ.png?​400 |}}+<​WRAP ​column 48%> {{:​resources:​eval:​dpg:​ad9129:​figure12b_9129-MIX-EBZ.png?​400 |}}
 </​WRAP>​ </​WRAP>​
-<​WRAP ​right 50%> {{:​resources:​eval:​dpg:​ad9129:​figure12a_9129-MIX-EBZ.png?​400 |}}+<​WRAP ​column 48%> {{:​resources:​eval:​dpg:​ad9129:​figure12a_9129-MIX-EBZ.png?​400 |}}
 </​WRAP>​ </​WRAP>​
 <WRAP clear> <WRAP clear>
resources/eval/dpg/ad9119-mix-ebz.1350066874.txt.gz · Last modified: 12 Oct 2012 20:34 by Dan Fague