This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:dpg:ad9119-mix-ebz [15 Oct 2012 17:04] Dan Fague removing under construction tag |
resources:eval:dpg:ad9119-mix-ebz [02 Nov 2012 20:38] Dan Fague [Mix-Mode Operation] |
||
---|---|---|---|
Line 18: | Line 18: | ||
- | <WRAP col2 50%> | + | <WRAP column 40%> |
{{:resources:eval:dpg:ad9129:bench_setup_9119_evb.png?350 |}} | {{:resources:eval:dpg:ad9129:bench_setup_9119_evb.png?350 |}} | ||
</WRAP> | </WRAP> | ||
- | <WRAP right 50%> | + | <WRAP column 55%> |
{{:resources:eval:dpg:ad9129:figure2_9129-MIX-EBZ.png?400 |}} | {{:resources:eval:dpg:ad9129:figure2_9129-MIX-EBZ.png?400 |}} | ||
</WRAP> | </WRAP> | ||
<WRAP clear> | <WRAP clear> | ||
</WRAP> | </WRAP> | ||
- | <WRAP col2 50%> | + | <WRAP column 40%> |
Figure 1 - Block diagram of the AD9119 lab bench set-up | Figure 1 - Block diagram of the AD9119 lab bench set-up | ||
</WRAP> | </WRAP> | ||
- | <WRAP right 50%> | + | <WRAP column 55%> |
Figure 2 - Top view of AD9119-MIX-EBZ Evaluation Board (uses the AD9129 EVB) | Figure 2 - Top view of AD9119-MIX-EBZ Evaluation Board (uses the AD9129 EVB) | ||
</WRAP> | </WRAP> | ||
Line 118: | Line 118: | ||
When using mix-mode and targeting a signal to the second Nyquist zone, it is important to remember that the center frequency chosen in the DPG window is the offset from the DACCLK sample frequency, not 0 Hz. For example, to place the carrier at 1982.5 MHz with a 2.4576 GHz DACCLK as in Figure 12, program the DPG Downloader center frequency to 475 MHz and enable mix-mode. Figure 12 shows the IMD performance of several different DAC output currents and the loss in output power expected with lower currents. | When using mix-mode and targeting a signal to the second Nyquist zone, it is important to remember that the center frequency chosen in the DPG window is the offset from the DACCLK sample frequency, not 0 Hz. For example, to place the carrier at 1982.5 MHz with a 2.4576 GHz DACCLK as in Figure 12, program the DPG Downloader center frequency to 475 MHz and enable mix-mode. Figure 12 shows the IMD performance of several different DAC output currents and the loss in output power expected with lower currents. | ||
- | <WRAP col2 50%> {{:resources:eval:dpg:ad9129:figure12b_9129-MIX-EBZ.png?400 |}} | + | <WRAP column 48%> {{:resources:eval:dpg:ad9129:figure12b_9129-MIX-EBZ.png?400 |}} |
</WRAP> | </WRAP> | ||
- | <WRAP right 50%> {{:resources:eval:dpg:ad9129:figure12a_9129-MIX-EBZ.png?400 |}} | + | <WRAP column 48%> {{:resources:eval:dpg:ad9129:figure12a_9129-MIX-EBZ.png?400 |}} |
</WRAP> | </WRAP> | ||
<WRAP clear> | <WRAP clear> |