This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:dpg:ad9119-mix-ebz [12 Oct 2012 20:34] – [Hardware Setup] Dan Fague | resources:eval:dpg:ad9119-mix-ebz [02 Nov 2012 20:38] (current) – [Mix-Mode Operation] Dan Fague | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ~~UNDERCONSTRUCTION~~ | ||
====== AD9119-MIX-EBZ Evaluation Board Quick Start Guide ====== | ====== AD9119-MIX-EBZ Evaluation Board Quick Start Guide ====== | ||
===== Getting Started with the AD9119 Mix-mode(tm) Evaluation Board and Software ===== | ===== Getting Started with the AD9119 Mix-mode(tm) Evaluation Board and Software ===== | ||
Line 19: | Line 18: | ||
- | < | + | < |
{{: | {{: | ||
</ | </ | ||
- | < | + | < |
{{: | {{: | ||
</ | </ | ||
<WRAP clear> | <WRAP clear> | ||
</ | </ | ||
- | < | + | < |
Figure 1 - Block diagram of the AD9119 lab bench set-up | Figure 1 - Block diagram of the AD9119 lab bench set-up | ||
</ | </ | ||
- | < | + | < |
Figure 2 - Top view of AD9119-MIX-EBZ Evaluation Board (uses the AD9129 EVB) | Figure 2 - Top view of AD9119-MIX-EBZ Evaluation Board (uses the AD9129 EVB) | ||
</ | </ | ||
Line 119: | Line 118: | ||
When using mix-mode and targeting a signal to the second Nyquist zone, it is important to remember that the center frequency chosen in the DPG window is the offset from the DACCLK sample frequency, not 0 Hz. For example, to place the carrier at 1982.5 MHz with a 2.4576 GHz DACCLK as in Figure 12, program the DPG Downloader center frequency to 475 MHz and enable mix-mode. Figure 12 shows the IMD performance of several different DAC output currents and the loss in output power expected with lower currents. | When using mix-mode and targeting a signal to the second Nyquist zone, it is important to remember that the center frequency chosen in the DPG window is the offset from the DACCLK sample frequency, not 0 Hz. For example, to place the carrier at 1982.5 MHz with a 2.4576 GHz DACCLK as in Figure 12, program the DPG Downloader center frequency to 475 MHz and enable mix-mode. Figure 12 shows the IMD performance of several different DAC output currents and the loss in output power expected with lower currents. | ||
- | < | + | < |
</ | </ | ||
- | < | + | < |
</ | </ | ||
<WRAP clear> | <WRAP clear> |