This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:dpg:ace_ad9144-fmc-ebz [12 Aug 2022 11:46] – [Quick Start Guide] Shine Cabatan | resources:eval:dpg:ace_ad9144-fmc-ebz [12 Aug 2022 11:51] (current) – [Quick Start Guide] Shine Cabatan | ||
---|---|---|---|
Line 54: | Line 54: | ||
===== Quick Start Guide ===== | ===== Quick Start Guide ===== | ||
- | - Attach AD9144-FMC-EBZ onto the FMC connector of ADS7-V2 controller board. Connect the evaluation board to PC via USB, the continuous waveform generator output to J1, and one of the DAC outputs (J4/ | + | - Attach AD9144-FMC-EBZ onto the FMC connector of ADS7-V2 controller board. Connect the evaluation board to PC via USB, the continuous waveform generator output to J1, and one of the DAC outputs (J4/ |
- Set the frequency of the continuous waveform generator output to **1.5 GHz** and the output level to **+3 dBm**. Enable the output. <WRAP centeralign> | - Set the frequency of the continuous waveform generator output to **1.5 GHz** and the output level to **+3 dBm**. Enable the output. <WRAP centeralign> | ||
- Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**, | - Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**, | ||
Line 73: | Line 73: | ||
* **Generate Complex Data (I & Q):** checked <insert DPG screenshot with lane rate and synced status> | * **Generate Complex Data (I & Q):** checked <insert DPG screenshot with lane rate and synced status> | ||
- In the ADS7-V2 panel in the DPG window, configure **Data Playback** by selecting tones for the DAC outputs from each dropdown menu. Set **JESD Mode** to Mode 0, **Links** to Single, and **Subclass** to 0.<WRAP centeralign> | - In the ADS7-V2 panel in the DPG window, configure **Data Playback** by selecting tones for the DAC outputs from each dropdown menu. Set **JESD Mode** to Mode 0, **Links** to Single, and **Subclass** to 0.<WRAP centeralign> | ||
- | - Press the download arrow ({{: | + | - Press the download arrow ({{: |