Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:dpg:ace_ad9144-fmc-ebz [12 Aug 2022 11:48] – [Quick Start Guide] Shine Cabatanresources:eval:dpg:ace_ad9144-fmc-ebz [12 Aug 2022 11:51] (current) – [Quick Start Guide] Shine Cabatan
Line 54: Line 54:
 ===== Quick Start Guide ===== ===== Quick Start Guide =====
  
-  - Attach AD9144-FMC-EBZ onto the FMC connector of ADS7-V2 controller board. Connect the evaluation board to PC via USB, the continuous waveform generator output to J1, and one of the DAC outputs (J4/J5/J14/J17) to a signal/spectrum analyzer. Connect ADS7-V2 to PC via USB and to a 12V 60W AC/DC power supply, then switch the board ON using S1 beside the connector for 12V supply. Refer to [[:resources:eval:dpg:ad9144-fmc-ebz?rev=1660297596#typical setup|Typical Setup]] section for pictures of actual evaluation setup.+  - Attach AD9144-FMC-EBZ onto the FMC connector of ADS7-V2 controller board. Connect the evaluation board to PC via USB, the continuous waveform generator output to J1, and one of the DAC outputs (J4/J5/J14/J17) to a signal/spectrum analyzer. Connect ADS7-V2 to PC via USB and to a 12V 60W AC/DC power supply, then switch the board ON using S1 beside the connector for 12V supply. Refer to [[:resources:eval:dpg:ace_ad9144-fmc-ebz#typical setup|Typical Setup]] section for pictures of actual evaluation setup.
   - Set the frequency of the continuous waveform generator output to **1.5 GHz** and the output level to **+3 dBm**. Enable the output. <WRAP centeralign>{{ :resources:eval:dpg:ad9144-fmc-ebz_dpg_board_detect.png?600 |}}//Figure 2. ADS7-V2 and AD9144 detected in DPG Software//</WRAP>   - Set the frequency of the continuous waveform generator output to **1.5 GHz** and the output level to **+3 dBm**. Enable the output. <WRAP centeralign>{{ :resources:eval:dpg:ad9144-fmc-ebz_dpg_board_detect.png?600 |}}//Figure 2. ADS7-V2 and AD9144 detected in DPG Software//</WRAP>
   - Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**, respectively. See Figure 2. <WRAP centeralign>{{ :resources:eval:dpg:ad9144-fmc-ebz_ace_board_detect.png?600 |}}//Figure 3. AD9144-FMC-EBZ detected in ACE//</WRAP>   - Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**, respectively. See Figure 2. <WRAP centeralign>{{ :resources:eval:dpg:ad9144-fmc-ebz_ace_board_detect.png?600 |}}//Figure 3. AD9144-FMC-EBZ detected in ACE//</WRAP>
Line 73: Line 73:
     * **Generate Complex Data (I & Q):** checked <insert DPG screenshot with lane rate and synced status>     * **Generate Complex Data (I & Q):** checked <insert DPG screenshot with lane rate and synced status>
   - In the ADS7-V2 panel in the DPG window, configure **Data Playback** by selecting tones for the DAC outputs from each dropdown menu. Set **JESD Mode** to Mode 0, **Links** to Single, and **Subclass** to 0.<WRAP centeralign>{{ :resources:eval:dpg:ad9144-fmc-ebz_spectrum_capture.png?600 |}}//Figure 7. AD9144 DAC Output FFT for Data Rate = 750 MHz, FOUT = 112 MHz//</WRAP>   - In the ADS7-V2 panel in the DPG window, configure **Data Playback** by selecting tones for the DAC outputs from each dropdown menu. Set **JESD Mode** to Mode 0, **Links** to Single, and **Subclass** to 0.<WRAP centeralign>{{ :resources:eval:dpg:ad9144-fmc-ebz_spectrum_capture.png?600 |}}//Figure 7. AD9144 DAC Output FFT for Data Rate = 750 MHz, FOUT = 112 MHz//</WRAP>
-  - Press the download arrow ({{:resources:eval:dpg:9154_down_arrow.png}}) then the play button ({{:resources:eval:dpg:9154_right_green_arrow.png}}). **Serial Line Rate** should appear as <> Gbps and **Sync Status** should have a check mark. FFT plot of the DAC output is in Figure 7.+  - Press the download arrow ({{:resources:eval:dpg:9154_down_arrow.png}}) then the play button ({{:resources:eval:dpg:9154_right_green_arrow.png}}). **Serial Line Rate** should appear as 7.5 Gbps and **Sync Status** should have a check mark. FFT plot of the DAC output is in Figure 7.
  
  
  
  
resources/eval/dpg/ace_ad9144-fmc-ebz.txt · Last modified: 12 Aug 2022 11:51 by Shine Cabatan