Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:dpg:ace_ad9144-fmc-ebz [12 Aug 2022 11:51]
Shine Cabatan old revision restored (12 Aug 2022 11:46)
resources:eval:dpg:ace_ad9144-fmc-ebz [12 Aug 2022 11:51] (current)
Shine Cabatan [Quick Start Guide]
Line 73: Line 73:
     * **Generate Complex Data (I & Q):** checked <insert DPG screenshot with lane rate and synced status>     * **Generate Complex Data (I & Q):** checked <insert DPG screenshot with lane rate and synced status>
   - In the ADS7-V2 panel in the DPG window, configure **Data Playback** by selecting tones for the DAC outputs from each dropdown menu. Set **JESD Mode** to Mode 0, **Links** to Single, and **Subclass** to 0.<WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9144-fmc-ebz_spectrum_capture.png?​600 |}}//Figure 7. AD9144 DAC Output FFT for Data Rate = 750 MHz, FOUT = 112 MHz//</​WRAP>​   - In the ADS7-V2 panel in the DPG window, configure **Data Playback** by selecting tones for the DAC outputs from each dropdown menu. Set **JESD Mode** to Mode 0, **Links** to Single, and **Subclass** to 0.<WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9144-fmc-ebz_spectrum_capture.png?​600 |}}//Figure 7. AD9144 DAC Output FFT for Data Rate = 750 MHz, FOUT = 112 MHz//</​WRAP>​
-  - Press the download arrow ({{:​resources:​eval:​dpg:​9154_down_arrow.png}}) then the play button ({{:​resources:​eval:​dpg:​9154_right_green_arrow.png}}). **Serial Line Rate** should appear as <> ​Gbps and **Sync Status** should have a check mark. FFT plot of the DAC output is in Figure 7.+  - Press the download arrow ({{:​resources:​eval:​dpg:​9154_down_arrow.png}}) then the play button ({{:​resources:​eval:​dpg:​9154_right_green_arrow.png}}). **Serial Line Rate** should appear as 7.5 Gbps and **Sync Status** should have a check mark. FFT plot of the DAC output is in Figure 7.
  
  
  
  
resources/eval/dpg/ace_ad9144-fmc-ebz.txt · Last modified: 12 Aug 2022 11:51 by Shine Cabatan