Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:dpg:ace_ad9136-ebz [18 Mar 2016 21:19] – [AD9136/AD9135 Evaluation Software] Michele Viani | resources:eval:dpg:ace_ad9136-ebz [29 Dec 2020 20:38] (current) – fix links Robin Getz |
---|
===== Getting Started with the AD9136/AD9135-EBZ Evaluation Board and Software ===== | ===== Getting Started with the AD9136/AD9135-EBZ Evaluation Board and Software ===== |
==== What's in the Box ==== | ==== What's in the Box ==== |
* [[adi>AD9136/AD9135-EBZ]] Evaluation Board | * [[adi>EVAL-AD9135]] or [[adi>EVAL-AD9136]] Evaluation Board for the [[adi>AD9136]]/[[adi>AD9135]] |
* Evaluation Board CD | * Evaluation Board CD |
* Mini-USB Cable | * Mini-USB Cable |
| |
===== Introduction ====== | ===== Introduction ====== |
The AD9136/AD9135-EBZ connects to a DPG3 for quick evaluation of the [[adi>AD9136/AD9135]], a high-speed, signal processing Digital to Analog Converter. The DPG3 automatically formats the data and sends it to the AD9136/AD9135-EBZ, simplifying evaluation of the device. The Evaluation Board (EVB) runs from a +5V supply. A clock distribution chip AD9516 is included on this EVB as a clock fan-out and frequency divider for the DACCLK, REFCLK and DPG3 input clock. Figure 2 is an image of the top side of the AD9136-EBZ. | The AD9136/AD9135-EBZ connects to a DPG3 for quick evaluation of the [[adi>AD9136]]/[[adi>AD9135]], a high-speed, signal processing Digital to Analog Converter. The DPG3 automatically formats the data and sends it to the AD9136/AD9135-EBZ, simplifying evaluation of the device. The Evaluation Board (EVB) runs from a +5V supply. A clock distribution chip AD9516 is included on this EVB as a clock fan-out and frequency divider for the DACCLK, REFCLK and DPG3 input clock. Figure 2 is an image of the top side of the AD9136-EBZ. |
===== AD9136/AD9135 Evaluation Software ===== | ===== AD9136/AD9135 Evaluation Software ===== |
The AD9136/AD9135 Evaluation Board software runs on the easy-to-use ACE (Analysis|Control|Evaluate) graphical user interface (GUI). It is included on the Evaluation Board CD. Registers on the AD9136/AD9135 and AD9516 products are programmed via a USB cable connecting the user’s PC to the AD9144-EBZ XP2 connector. Software in the AD9136-EBZ/AD9135-EBZ PIC processor (XU1) provides the interface between the USB bus and the SPI busses of the AD9136/AD9135 and AD9516. | The AD9136/AD9135 Evaluation Board software runs on the easy-to-use ACE (Analysis|Control|Evaluate) graphical user interface (GUI). It is included on the Evaluation Board CD. Registers on the AD9136/AD9135 and AD9516 products are programmed via a USB cable connecting the user’s PC to the AD9144-EBZ XP2 connector. Software in the AD9136-EBZ/AD9135-EBZ PIC processor (XU1) provides the interface between the USB bus and the SPI busses of the AD9136/AD9135 and AD9516. |
=== Configure DPG Vector Software === | === Configure DPG Vector Software === |
1. To begin, turn on the external +5V supply. \\ \\ | 1. To begin, turn on the external +5V supply. \\ \\ |
2. Open DPG Downloader if you have not done so. (Start > All Programs > Analog Devices > DPG > DPGDownloader). Ensure that the program detects the AD9136/AD9135, as indicated in the “Evaluation Board” drop-down list, and select it. Select "QBF 2X4 85G 425M" from the "Port Configuration" drop-down list and "Mode 8" from the "JESD Mode" drop-down list. \\ \\ | 2. Open DPG Downloader if you have not done so. (Start > All Programs > Analog Devices > DPG > DPGDownloader). Ensure that the program detects the AD9136/AD9135, as indicated in the “Evaluation Board” drop-down list, shown in Figure 3. |
| <WRAP center> |
| | {{ {{ :resources:eval:dpg:ad9136:AD9136-EBZ_DPGStartup.png?600 |}} | |
| | Figure 3. Initial DPGDownloader Panel | |
| </WRAP> |
| 3. Select "QBF 2X4 85G 425M" from the "Port Configuration" drop-down list to configure the DPG for Dual Link and "Mode 8" from the "JESD Mode" drop-down list. \\ \\ |
3. Click on “Add Generated Waveform”, and then “Wireless Infrastructure”. A WIFR panel will be added to the vector list. Enter the Data Rate, in this case 1.6GHz and the desired frequency, 100MHz. Enter the digital amplitude. In this case we use 0dBFS. Select "2's Complement" from the Number Format drop-down list. Input the center frequency of "100MHz" at the bottom of the panel, choose "WCDMA" from the Standard drop-down menu and increase the No. of Carriers to "4" - then hit the "Add Carriers" button. The DPG Downloader panel should look like Figure 3. \\ \\ | 3. Click on “Add Generated Waveform”, and then “Wireless Infrastructure”. A WIFR panel will be added to the vector list. Enter the Data Rate, in this case 1.6GHz and the desired frequency, 100MHz. Enter the digital amplitude. In this case we use 0dBFS. Select "2's Complement" from the Number Format drop-down list. Input the center frequency of "100MHz" at the bottom of the panel, choose "WCDMA" from the Standard drop-down menu and increase the No. of Carriers to "4" - then hit the "Add Carriers" button. The DPG Downloader panel should look like Figure 3. \\ \\ |
4. Select the WIFR vector (I) in the “DAC0” drop down menu and the WIFR vector (Q) in the “DAC1”. At this point, the DPG Downloader panel should look like Figure 3.\\ \\ | 4. Select the WIFR vector (I) in the “DAC0” drop down menu and the WIFR vector (Q) in the “DAC1”. At this point, the DPG Downloader panel should look like Figure 4.\\ \\ |
| |
<WRAP center> | <WRAP center> |
| {{ {{ :resources:eval:dpg:ad9136:ad9136-ebz_dpg_finalview.png?600 |}}}} | | | {{ {{ :resources:eval:dpg:ad9136:AD9136-EBZ_DPGSetup.png?600 |}} | |
| Figure 3. DPG Downloader Panel | | | Figure 4. Configured DPGDownloader Panel | |
</WRAP> | </WRAP> |
| |
=== Configuring SPI === | === Configuring SPI === |
| |
1. Open the AD9136/AD9135 SPI application (Start > All Programs > Analog Devices > AD9136/AD9135 > AD9136/AD9135 SPI). The screen should look similar to Figure 4. \\ \\ | 1. Open ACE (Start > All Programs > Analog Devices > ACE). It should recognize the AD9136-EBZ or AD9135-EBZ in the attached hardware section when the application startup screen displays, as showing in Figure 5 for the AD9136-EBZ. \\ \\ |
<WRAP center> | <WRAP center> |
| | {{ {{ :resources:eval:dpg:ad9136:AD9136-EBZ_ACEStartup.png?600 |}} | |
| {{ {{ :resources:eval:dpg:ad9136:ad9136-ebz_spipro_initialview.png?600 |}}|}} | | | Figure 5. Initial ACE Startup Window with Attached Hardware AD9136-EBZ | |
| |
| Figure 4. Entry Screen of the AD9136/AD9135 SPI software | | |
</WRAP> | </WRAP> |
| |
2. Configure the hardware according to the hardware set-up instructions given in the Hardware Setup section above. Set the frequency of the DAC clock signal generator to 1.6GHz, and the output level to 3dBm. The spectrum analyzer can be configured with Start Frequency = 1 MHz, Stop Frequency = 800 MHz, and Resolution Bandwidth of 30 kHz, and Trace Detector to Average (Log/RMS/V). Choose Input Attenuation to be 8dB. This can be adjusted later if indications are that the analyzer is causing degradations. \\ \\ | 2. Configure the hardware according to the hardware set-up instructions given in the Hardware Setup section above. Set the frequency of the DAC clock signal generator to 1.6GHz, and the output level to 3dBm. The spectrum analyzer can be configured with Start Frequency = 1 MHz, Stop Frequency = 800 MHz, and Resolution Bandwidth of 30 kHz, and Trace Detector to Average (Log/RMS/V). Choose Input Attenuation to be 8dB. This can be adjusted later if indications are that the analyzer is causing degradations. \\ \\ |
3. Follow the sequence below to configure the AD9136/AD9135 SPI registers. \\ \\ | 3. Follow the sequence below to configure the AD9136-EBZ/AD9135-EBZ Setup Wizard settings. \\ \\ |
a. The Links should be set to dual link. The JESD Mode is set to 8, Subclass 1 box checked, Interpolation set to 1, and FDAC set to 1.6GHz. Click “Commit” button to initialize the AD9136/AD9135. The JESD204B PLL should be locked indicated with bright green JESD204B PLL readback LED.\\ \\ | a. The Links should be set to dual link. The JESD Mode is set to 8, Interpolation set to 1, and FDAC set to 1.6GHz, as shown in Figure 6. |
b. At this point the Serial Line Rate in the DPG3 software panel should read 8Gbps.\\ \\ | |
| b. Hit “Apply” and the wizard will execute a startup routine to configure the AD9516 and the AD9136/AD9135. Once complete, the SERDES PLL lock indicator on the board will turn green if it locked and the display will look like Figure 7.\\ \\ |
| |
<WRAP center> | <WRAP center> |
| {{ {{ :resources:eval:dpg:ad9136:ad9136-ebz_spipro_finalview.png?600 |}} |}} | | | {{ {{ :resources:eval:dpg:ad9136:ad9136-ebz_ACESetup.png?600 |}} | |
| Figure 5. Configured panel of the AD9136/AD9135 SPI software | | | Figure 6. Configured ACE Wizard GUI for the AD9136-EBZ | |
| |
| | {{ {{ :resources:eval:dpg:ad9136:ad9136-ebz_ACEWizRan.png?600 |}} | |
| | Figure 7. ACE Wizard Executed and SERDES PLL Locked for the AD9136-EBZ | |
</WRAP> | </WRAP> |
| |
d. Click Download ({{:resources:eval:dpg:image009.png?direct&|}}) and Play ({{:resources:eval:dpg:image010.png?direct&|}}) in the DPG Downloader screen. \\ \\ | 4. Return to DPGDownloader and note the Serial Line Rate readback should read 8Gbps indicating that the clocks going to the FPGA are configured properly for this setup, as shown in Figure 8. |
| |
| 5. Click Download ({{:resources:eval:dpg:9154_down_arrow.png}}) and Play ({{:resources:eval:dpg:9154_right_green_arrow.png}}) in the DPGDownloader screen. \\ \\ |
| |
| <WRAP center> |
| | {{ {{ :resources:eval:dpg:ad9136:ad9136-ebz_DPGDwnld.png?600 |}} | |
| | Figure 8. Executed DPGDownloader GUI for the AD9136-EBZ | |
| </WRAP> |
| |
e. The current on the 5V supply should read about 1430mA. If you do not see the output, gently push the board toward the DPG3. This ensures that the board is firmly connected to the DPG3. The four registers codeGrpSync, FrameSync, GoodCheckSum and Initial LaneSync should all read 0F indicating the lanes are working correctly. \\ \\ | The current on the 5V supply should read about 1430mA. If you do not see the output, gently push the board toward the DPG3. This ensures that the board is firmly connected to the DPG3. The four register readbacks on the board view for Code Group Sync, Frame Sync, Good CheckSum and Initial Lane Sync should all read 0x0F indicating the lanes are working correctly, as seen in Figure 7. \\ \\ |
| |
3. The output spectrum of the DAC should look like Figure 6 below. | 6. The output spectrum of the DAC should look like Figure 9 below. |
<WRAP center> | <WRAP center> |
| {{ {{ :resources:eval:dpg:ad9136:ad9136_1.6ghzdac_1x_4xwcdma_fout100m_plloff.png?600 |}} |}} | | | {{ {{ :resources:eval:dpg:ad9136:ad9136_1.6ghzdac_1x_4xwcdma_fout100m_plloff.png?600 |}} | |
| Figure 6. AD9136/AD9135-EBZ Eval Board DAC output Spectrum | | | Figure 9. AD9136/AD9135-EBZ Eval Board DAC output Spectrum | |
</WRAP> | </WRAP> |
| |