This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:developer-kits:x-band-dev-kit:hardware-connections [17 May 2022 17:21] – Sam Ringwood | resources:eval:developer-kits:x-band-dev-kit:hardware-connections [17 May 2022 17:27] (current) – Sam Ringwood | ||
---|---|---|---|
Line 17: | Line 17: | ||
\\ | \\ | ||
==== RF Connectors ==== | ==== RF Connectors ==== | ||
- | - The Stingray board uses SMPM connectors on both sides of the board, so depending on how the board is used, adapters to mate with test equipment cabling may be required. Note that the Stingray board includes | + | - The Stingray board uses SMPM connectors on both sides of the board, so depending on how the board is used, adapters to mate with test equipment cabling may be required. Note that the Stingray board includes |
- | - The XUD1a board uses SMA connectors on the RF side of the board and SMPM connectors on the IF side of the board. | + | - The XUD1a board uses SMA connectors on the RF side of the board and SMPM connectors on the IF side of the board. Note that the XUD1A board includes 1x 12" SMPM-SMA cable. |
- The MxFE board uses SMA connectors for both the ADCs and DACs. | - The MxFE board uses SMA connectors for both the ADCs and DACs. | ||