This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:adr1399h-ebz [29 Oct 2021 01:11] – minor update to text Paul Blanchard | resources:eval:adr1399h-ebz [23 Nov 2021 00:58] (current) – [Features] Paul Blanchard | ||
---|---|---|---|
Line 19: | Line 19: | ||
**GENERAL DESCRIPTION** \\ | **GENERAL DESCRIPTION** \\ | ||
The ADR1399H-EBZ allows the evaluation of the ADR1399KHZ, ultra-stable 7.05V Shunt Voltage Reference in 4-lead TO-46 package. | The ADR1399H-EBZ allows the evaluation of the ADR1399KHZ, ultra-stable 7.05V Shunt Voltage Reference in 4-lead TO-46 package. | ||
- | The 4-layer board has had ground | + | |
+ | The DUT is elevated on its leads in order to increase the thermal isolation from the 4-layer board ground | ||
Isolated power means that the Reference output is effectively floated, removing the likelihood of ground loops. | Isolated power means that the Reference output is effectively floated, removing the likelihood of ground loops. | ||
The ultra-stable 7.05V is brought out to both banana jacks and to an edge mounted SMA connector. | The ultra-stable 7.05V is brought out to both banana jacks and to an edge mounted SMA connector. | ||
Line 30: | Line 32: | ||
Figure 1. ADR1399H-EBZ, | Figure 1. ADR1399H-EBZ, | ||
- | TABLE OF CONTENTS | ||
- | |||
- | Features 1 | ||
- | Evaluation Kit Contents 1 | ||
- | Equipment Needed 1 | ||
- | General Description 1 | ||
- | Evaluation Board Photograph 1 | ||
- | Revision History 2 | ||
- | Evaluation Board Quick Start Procedures 3 | ||
- | Power Supply Consideration 3 | ||
- | Initial Board Configuration 3 | ||
- | Using the Evaluation Board for Testing 3 | ||
- | Evaluation Board Schematic and Artwork 4 | ||
- | Ordering Information 6 | ||
- | Bill of Materials 6 | ||
- | |||
- | |||
- | |||
- | REVISION HISTORY | ||
- | 09/ | ||
- | 10/ | ||
- | 10/ | ||
- | |||
EVALUATION BOARD QUICK START PROCEDURES | EVALUATION BOARD QUICK START PROCEDURES | ||
- | The following sections outline the basic prepopulated configuration of the ADR1399H-EBZ required to test the basic functionality of the device. | + | The following sections outline the basic prepopulated configuration of the ADR1399H-EBZ required to test the basic functionality of the device. |
- | POWER SUPPLY CONSIDERATION | + | \\ |
- | Use a USB-C charger or other USB-C source to power the board. | + | POWER SUPPLY CONSIDERATION\\ |
- | INITIAL BOARD CONFIGURATION | + | Use a USB-C charger or other USB-C source to power the board. |
- | The ADR1399H-EBZ comes pre-configured. | + | \\ |
- | + | INITIAL BOARD CONFIGURATION\\ | |
- | USING THE EVALUATION BOARD FOR TESTING | + | The ADR1399H-EBZ comes pre-configured. |
- | The board was designed along the lines of a simple “pocket calibrator”, | + | \\ |
+ | USING THE EVALUATION BOARD FOR TESTING\\ | ||
+ | The board was designed along the lines of a simple “pocket calibrator”, | ||
- | The board is very easy to use. Just power the board using one of the methods discussed, and start measuring the output DC voltage. | + | The board is very easy to use. Just power the board using one of the methods discussed, and start measuring the output DC voltage. |
- | + | \\ | |
EVALUATION BOARD SCHEMATIC AND ARTWORK \\ | EVALUATION BOARD SCHEMATIC AND ARTWORK \\ | ||
{{: | {{: | ||
- | Figure 5. ADR1999H-EBZ Schematic, DUT Section\\ | + | Figure 5. ADR1399H-EBZ Schematic, DUT Section\\ |
{{: | {{: | ||
Line 99: | Line 80: | ||
©2019 Analog Devices, Inc. All rights reserved. Trademarks and | ©2019 Analog Devices, Inc. All rights reserved. Trademarks and | ||
| | ||
- | UG22920-0-12/ | + | |