This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:adf5610-ace-software-guide [07 May 2021 19:41] – [EDIT SWEEP AND HOP] Jude Osemene | resources:eval:adf5610-ace-software-guide [22 Jul 2021 19:19] (current) – [Software Installation Procedures] Jude Osemene | ||
---|---|---|---|
Line 4: | Line 4: | ||
You can install the EV-ADF5610SD1Z plug-in from the ACE start-up page. | You can install the EV-ADF5610SD1Z plug-in from the ACE start-up page. | ||
* You can install ACE from [[http:// | * You can install ACE from [[http:// | ||
- | * On the ACE start-up page locate and click the **Plug-in Manager** on the Side bar. | + | * On the ACE start-up page locate and click the **Plug-in Manager** on the side bar. |
+ | * Select Available Packages from the panel second side bar | ||
* Search for Board.ADF5610 and install plug-in | * Search for Board.ADF5610 and install plug-in | ||
+ | {{ : | ||
===== Evaluation Board Set-up ===== | ===== Evaluation Board Set-up ===== | ||
To run the plug-in, perform the following steps: | To run the plug-in, perform the following steps: |