Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:ada4355_evaluation_board [20 Sep 2021 17:32]
handa yukihisa Added "For Only Application Board User" section
resources:eval:ada4355_evaluation_board [20 Sep 2021 17:37] (current)
handa yukihisa [For Only Application Board User]
Line 87: Line 87:
 {{ :​resources:​eval:​toolbar_ada4355.png?​400 |}}\\ //Figure 20. Tool Bar//\\ {{ :​resources:​eval:​toolbar_ada4355.png?​400 |}}\\ //Figure 20. Tool Bar//\\
 =====For Only Application Board User ===== =====For Only Application Board User =====
-  * D23 in FMC Connector, which is labeled as "​1P8VA_EN",​ needs to be driven by more than 1.2V to make the ADA4355 Application board work properly.  ​+  * D23 in the FMC Connector, which is labeled as "​1P8VA_EN",​ needs to be driven by more than 1.2V to make the ADA4355 Application board work properly.  ​
 ======Downloads====== ​ ======Downloads====== ​
 <WRAP round 50% download>​ <WRAP round 50% download>​
resources/eval/ada4355_evaluation_board.txt · Last modified: 20 Sep 2021 17:37 by handa yukihisa