Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:ad9695-1300ebz [29 Aug 2019 20:20] – [Configuring the Board] Judy Chuiresources:eval:ad9695-1300ebz [14 Jan 2021 05:11] (current) – user interwiki links Robin Getz
Line 1: Line 1:
 ======= EVALUATING THE AD9695/AD9697 ANALOG-TO-DIGITAL CONVERTER ======= ======= EVALUATING THE AD9695/AD9697 ANALOG-TO-DIGITAL CONVERTER =======
 ====== Preface ====== ====== Preface ======
-This user guide describes the [[adi>AD9695|AD9695-1300EBZ]] evaluation board which provides all of the support circuitry required to operate the [[adi>AD9695|AD9695]] in its various modes and configurations. The [[adi>AD9697|AD9697]] ADC can be evaluated using the [[adi>AD9695|AD9695-1300EBZ]] evaluation board as well as the performance is identical except for power comsumption. This guide entails both the hardware and software setup needed to acquire data capture from the evaluation board. This guide assumes the usage of the accompanying [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-ADS7-V2|ADS7-V2 EBZ High Speed Evaluation Board]]. The user guide for the [[resources/eval/ads7-v2|ADS7-V2]] provides additional information available for consultation during usage. Documents and software tools, where available, can be found at the [[adi>hsadcevalboard|HS-ADC Eval Board homepage]]. For additional information or questions, post a question on [[https://ez.analog.com/community/data_converters |Engineer Zone]], or send an email to **highspeed.converters@analog.com**. <WRAP> </WRAP> <WRAP> </WRAP> <WRAP> </WRAP> <WRAP> </WRAP> <WRAP> </WRAP> <WRAP> </WRAP> <WRAP> </WRAP> <WRAP> </WRAP>+This user guide describes the [[adi>AD9695|AD9695-1300EBZ]] evaluation board which provides all of the support circuitry required to operate the [[adi>AD9695|AD9695]] in its various modes and configurations. The [[adi>AD9697|AD9697]] ADC can be evaluated using the [[adi>AD9695|AD9695-1300EBZ]] evaluation board as well as the performance is identical except for power comsumption. This guide entails both the hardware and software setup needed to acquire data capture from the evaluation board. This guide assumes the usage of the accompanying [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-ADS7-V2|ADS7-V2 EBZ High Speed Evaluation Board]]. The user guide for the [[resources/eval/ads7-v2|ADS7-V2]] provides additional information available for consultation during usage. Documents and software tools, where available, can be found at the [[adi>hsadcevalboard|HS-ADC Eval Board homepage]]. For additional information or questions, post a question on [[ez>community/data_converters |Engineer Zone]], or send an email to **highspeed.converters@analog.com**. <WRAP> </WRAP> <WRAP> </WRAP> <WRAP> </WRAP> <WRAP> </WRAP> <WRAP> </WRAP> <WRAP> </WRAP> <WRAP> </WRAP> <WRAP> </WRAP>
    
  
resources/eval/ad9695-1300ebz.txt · Last modified: 14 Jan 2021 05:11 by Robin Getz