Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:ad9680-1000ebz [17 Nov 2022 03:10]
John Xavier Toledo [Troubleshooting Tips]
resources:eval:ad9680-1000ebz [17 Nov 2022 03:13] (current)
John Xavier Toledo [Equipment Needed]
Line 64: Line 64:
   * Analog signal source and antialiasing filter   * Analog signal source and antialiasing filter
   * Sample clock source ​   * Sample clock source ​
-  * 12V, 6.5A switching power supply (such as the SL POWER CENB1080A1251F01 supplied with [[ads7-v2|ADS7-V2EBZ]])+  * 12V, 6.5A switching power supply (such as the SL POWER CENB1080A1251F01 supplied with [[adi>​eval-ads7-v2|ADS7-V2EBZ]])
   * PC running Windows®   * PC running Windows®
   * USB 2.0 port   * USB 2.0 port
resources/eval/ad9680-1000ebz.txt · Last modified: 17 Nov 2022 03:13 by John Xavier Toledo