Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:eval:ad9525-user-guide [30 Mar 2015 16:56] – [AD9525 Evaluation Board User Guide] Kyle Slightom | resources:eval:ad9525-user-guide [03 Jan 2021 22:11] (current) – fix links Robin Getz |
---|
* [[adi>eval-ad9525|AD9525 evaluation board software]] | * [[adi>eval-ad9525|AD9525 evaluation board software]] |
Documents Needed | Documents Needed |
* [[http://www.analog.com/static/imported-files/data_sheets/AD9525.pdf|AD9525 Datasheet]] | * [[adi>static/imported-files/data_sheets/AD9525.pdf|AD9525 Datasheet]] |
| |
===== GENERAL DESCRIPTION ===== | ===== GENERAL DESCRIPTION ===== |
---- | ---- |
The AD9525 quick start guide is intended for direct use with the AD9525/PCBZ-VCO evaluation board containing a prepopulated Z-COMM CRO2950B-LF external VCO. Although the AD9525/PCBZ can be populated with a different external VCO/VCXO, the settings discussed in this quick start guide may not be directly applicable. This guide covers only simple PLL operation to lock the PLL. See the AD9525 data sheet and the Evaluation Software Components section for a detailed explanation of the various AD9525 features.\\ \\ | The AD9525 quick start guide is intended for direct use with the AD9525/PCBZ-VCO evaluation board containing a prepopulated Z-COMM CRO2950B-LF external VCO. Although the AD9525/PCBZ can be populated with a different external VCO/VCXO, the settings discussed in this quick start guide may not be directly applicable. This guide covers only simple PLL operation to lock the PLL. See the AD9525 data sheet and the Evaluation Software Components section for a detailed explanation of the various AD9525 features.\\ \\ |
The AD9525 website contains a setup file to configure the AD9525/PCBZ-VCO to the settings discussed in this section. The setup file can be found online [[http://www.analog.com/en/clock-and-timing/clock-generation-and-distribution/ad9525/products/EVAL-AD9525/eb.html|here]]. After being downloaded, the setup file can be loaded into the evaluation board by opening the AD9525 evaluation software, selecting Load Setup from the File menu, and selecting the appropriate .stp file. The values in Table 5 are used for the example discussed in the Quick Start Steps section.\\ \\ | The AD9525 website contains a setup file to configure the AD9525/PCBZ-VCO to the settings discussed in this section. The setup file can be found online [[adi>en/clock-and-timing/clock-generation-and-distribution/ad9525/products/EVAL-AD9525/eb.html|here]]. After being downloaded, the setup file can be loaded into the evaluation board by opening the AD9525 evaluation software, selecting Load Setup from the File menu, and selecting the appropriate .stp file. The values in Table 5 are used for the example discussed in the Quick Start Steps section.\\ \\ |
| |
<WRAP column 48%> | <WRAP column 48%> |