This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:ad9467-fmc-250ebz [09 Jan 2021 00:22] – user interwiki links Robin Getz | resources:eval:ad9467-fmc-250ebz [05 Oct 2021 23:05] – Added AD9517 setup instructions, updated ftp links Alex Arrants | ||
---|---|---|---|
Line 30: | Line 30: | ||
* [[adi> | * [[adi> | ||
===== Software Needed ===== | ===== Software Needed ===== | ||
- | * VisualAnalog | + | * [[adi> |
- | * SPIController | + | * [[adi>/en/design-center/interactive-design-tools/spicontroller.html|SPIController]] |
+ | | ||
===== Design and Integration Files ===== | ===== Design and Integration Files ===== | ||
- | * FPGA BIN file ftp:// | + | * {{: |
* [[/ | * [[/ | ||
===== Equipment Needed ===== | ===== Equipment Needed ===== | ||
Line 106: | Line 107: | ||
* Ensure that the ADC has a valid clock input | * Ensure that the ADC has a valid clock input | ||
+ | ===== AD9517-4 Configuration (Optional) ===== | ||
+ | The AD9467-FMC-250EBZ is configured from the factory to use an external clock connected to J201. Alternatively, | ||
+ | |||
+ | ** Hardware Modifications ** | ||
+ | | ||
+ | *Add the following components: C205, C206, C300, C301, C304, C305 | ||
+ | *Make sure that Jumper P200 is on the " | ||
+ | |||
+ | **Additional Software Needed** | ||
+ | | ||
+ | ** Setup Instructions ** | ||
+ | - Make sure that a clock source is not connected to J201 | ||
+ | - Configure SPIcontroller and VisualAnalog as described above | ||
+ | - Launch a 2nd instance of SPIController. | ||
+ | - Load the AD9517spiR03.cfg configuration file. | ||
+ | - Click Config> | ||
+ | - Select " | ||
+ | //Figure 12. Select Fifo Chip Sel # 2 in SPIController//</ | ||
+ | - Click Apply and OK | ||
+ | - Click File> | ||
+ | - Select the configure_ad9517_AD9467-FMC-250EBZ .mgp file | ||
+ | - Check the Enable Check Box {{ : | ||
+ | //Figure 13. Select Enable Macro in SPIController//</ | ||
+ | - Click Run Macros {{ : | ||
+ | //Figure 14. Click Run Macros in SPIController//</ | ||
+ | - Make sure that LED CR300 is illuminated on the AD9467-FMC-250EBZ. | ||
+ | |||
+ | ** Obtaining an FFT ** | ||
+ | - Click the Run button in VisualAnalog , you should see the captured data similar to the plot shown in Figure 9 {{ : | ||
+ | //Figure 15. AD9467-FMC-250 FFT at 140.3MHz Analog Input (performance may be degraded compared to high-quality direct clock)//</ | ||