Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:ad9266-80ebz_ad9649-80ebz_ad9629-80ebz_ad9609-80ebz [03 Jun 2015 19:39] – Added external trigger documents for AD9649_29_09 Doug Itoresources:eval:ad9266-80ebz_ad9649-80ebz_ad9629-80ebz_ad9609-80ebz [04 May 2016 17:28] (current) Doug Ito
Line 107: Line 107:
 ===== Modes of Operation ===== ===== Modes of Operation =====
 ==== Standalone (PIN) Mode ==== ==== Standalone (PIN) Mode ====
-The [[adi>AD9266|AD9266]]/[[adi>AD9649|AD9649]]/[[adi>AD9629|AD9629]]/[[adi>AD9609|AD9609]] ADCs can operate in pin mode if there is no need to program and change the default modes of operation via the SPI. For applications that do not require SPI mode operation, the CSB pin is tied to 1.8V_DUT_AVDD by removing any jumper on Pin 8 of J302. In this configuration, the SDIO/PDWN pin controls the power-down function, and the SCLK/DFS pin controls the digital output format. \\+The [[adi>AD9266|AD9266]]/[[adi>AD9649|AD9649]]/[[adi>AD9629|AD9629]]/[[adi>AD9609|AD9609]] ADCs can operate in pin mode if there is no need to program and change the default modes of operation via the SPI. For applications that do not require SPI mode operation, the CSB pin is tied to AUX_DVDD by removing any jumper on Pin 8 of J302. In this configuration, the SDIO/PDWN pin controls the power-down function, and the SCLK/DFS pin controls the digital output format. \\
 \\ \\
 Table 2 and Table 3 specify the settings for pin mode operation. (These settings apply only when CSB is tied high, that is, J302 Pin 8 has no jumper.) Table 2 and Table 3 specify the settings for pin mode operation. (These settings apply only when CSB is tied high, that is, J302 Pin 8 has no jumper.)
resources/eval/ad9266-80ebz_ad9649-80ebz_ad9629-80ebz_ad9609-80ebz.txt · Last modified: 04 May 2016 17:28 by Doug Ito