This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:ad9259-50ebz [03 Dec 2021 04:26] Meriam Yuson-Aguila [Configuring the Board] |
resources:eval:ad9259-50ebz [03 Dec 2021 04:28] Meriam Yuson-Aguila [Equipment Needed] |
||
---|---|---|---|
Line 9: | Line 9: | ||
{{ :resources:eval:ad9259_set-up.jpg?600 |}} | {{ :resources:eval:ad9259_set-up.jpg?600 |}} | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | //Figure 1. Evaluation Board Connection—[[adi>AD9228|AD9228-65EBZ]], [[adi>AD9259|AD9259-50EBZ]] or [[adi>AD9287|AD9287-100EBZ]] (on Left) and [[adi>hsadcevalboard|HSC-ADC-EVALCZ]] (on Right)// | + | //Figure 1. Evaluation Board Connection—[[adi>AD9228|AD9228-65KITZ]], [[adi>AD9259|AD9259-50KITZ]] or [[adi>AD9287|AD9287-100KITZ]] (on Left) and [[adi>hsadcevalboard|HSC-ADC-EVALCZ]] (on Right)// |
</WRAP> | </WRAP> | ||
Line 34: | Line 34: | ||
* PC running Windows® | * PC running Windows® | ||
* USB 2.0 port, recommended (USB 1.1-compatible) | * USB 2.0 port, recommended (USB 1.1-compatible) | ||
- | * [[adi>AD9228|AD9228-65EBZ]], [[adi>AD9259|AD9259-50EBZ]] or [[adi>AD9287|AD9287-100EBZ]] | + | * [[adi>AD9228|AD9228-65KITZ]], [[adi>AD9259|AD9259-50KITZ]] or [[adi>AD9287|AD9287-100KITZ]] |
* [[adi>hsadcevalboard|HSC-ADC-EVALCZ]] FPGA-based data capture kit | * [[adi>hsadcevalboard|HSC-ADC-EVALCZ]] FPGA-based data capture kit | ||