Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:ad9257-65ebz_ad9637-80ebz [18 May 2016 00:16] – Minor Edit Doug Itoresources:eval:ad9257-65ebz_ad9637-80ebz [08 Jan 2021 10:50] (current) – Fixed bad link for AD9257 Ioana Chelaru
Line 59: Line 59:
 The evaluation board provides the support circuitry required to operate the [[adi>AD9257|AD9257]] and [[adi>AD9637|AD9637]] in their various modes and configurations. Figure 1 shows the typical bench characterization setup used to evaluate AC performance. It is critical that the signal sources used for the analog input and clock have very low phase noise (ideally ~100 fs rms jitter) to realize the optimum performance of the signal chain. Proper filtering of the analog input signal to remove harmonics and lower the integrated or broadband noise at the input is necessary to achieve the specified noise performance.\\  The evaluation board provides the support circuitry required to operate the [[adi>AD9257|AD9257]] and [[adi>AD9637|AD9637]] in their various modes and configurations. Figure 1 shows the typical bench characterization setup used to evaluate AC performance. It is critical that the signal sources used for the analog input and clock have very low phase noise (ideally ~100 fs rms jitter) to realize the optimum performance of the signal chain. Proper filtering of the analog input signal to remove harmonics and lower the integrated or broadband noise at the input is necessary to achieve the specified noise performance.\\ 
 \\  \\ 
-See [[adi>9257ce01a_designsupport|AD9257/9637 Design Support <Coming Soon>]] for the complete schematics and layout diagrams. These diagrams demonstrate the routing and grounding techniques that should be applied at the system level when designing application boards using these converters.\\+See [[adi>AD9257|AD9257/9637 Design Support <Coming Soon>]] for the complete schematics and layout diagrams. These diagrams demonstrate the routing and grounding techniques that should be applied at the system level when designing application boards using these converters.\\
  
 ==== Power Supplies ==== ==== Power Supplies ====
resources/eval/ad9257-65ebz_ad9637-80ebz.txt · Last modified: 08 Jan 2021 10:50 by Ioana Chelaru