Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:ad9253-125ebz_ad9633-125ebz [13 May 2013 18:57] – remove html syntax Doug Itoresources:eval:ad9253-125ebz_ad9633-125ebz [09 Jan 2021 00:22] (current) – user interwiki links Robin Getz
Line 55: Line 55:
 The evaluation board provides the support circuitry required to operate the [[adi>AD9653|AD9653]], [[adi>AD9253|AD9253]] and [[adi>AD9633|AD9633]] in their various modes and configurations. Figure 1 shows the typical bench characterization setup used to evaluate AC performance. It is critical that the signal sources used for the analog input and clock have very low phase noise (<1 ps rms jitter) to realize the optimum performance of the signal chain. Proper filtering of the analog input signal to remove harmonics and lower the integrated or broadband noise at the input is necessary to achieve the specified noise performance.\\  The evaluation board provides the support circuitry required to operate the [[adi>AD9653|AD9653]], [[adi>AD9253|AD9253]] and [[adi>AD9633|AD9633]] in their various modes and configurations. Figure 1 shows the typical bench characterization setup used to evaluate AC performance. It is critical that the signal sources used for the analog input and clock have very low phase noise (<1 ps rms jitter) to realize the optimum performance of the signal chain. Proper filtering of the analog input signal to remove harmonics and lower the integrated or broadband noise at the input is necessary to achieve the specified noise performance.\\ 
 \\  \\ 
-See the [[http://wiki.analog.com/resources/eval/ad9253-125ebz_ad9633-125ebz#getting_started|Getting Started]] section to get started, and visit [[adi>ug-328_designsupport|UG-328 Design Support]] for the complete schematics and layout diagrams. These diagrams demonstrate the routing and grounding techniques that should be applied at the system level when designing application boards using these converters.\\+See the [[/resources/eval/ad9253-125ebz_ad9633-125ebz#getting_started|Getting Started]] section to get started, and visit [[adi>ug-328_designsupport|UG-328 Design Support]] for the complete schematics and layout diagrams. These diagrams demonstrate the routing and grounding techniques that should be applied at the system level when designing application boards using these converters.\\
  
 ==== Power Supplies ==== ==== Power Supplies ====
resources/eval/ad9253-125ebz_ad9633-125ebz.txt · Last modified: 09 Jan 2021 00:22 by Robin Getz