This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:ad9208-3000ebz [27 Mar 2018 03:35] – [Preface] Umesh Jayamohan | resources:eval:ad9208-3000ebz [09 Jul 2018 15:11] – [Preface] Amrutha Anantha | ||
---|---|---|---|
Line 15: | Line 15: | ||
| <fc # | | <fc # | ||
+ | Note: ADS8-V1 does not support lane rates below 2Gbps. Hence, the following modes will not give a valid FFT. | ||
+ | LMF=411 and LMF=412 for a decimation ratio of 8 | ||
+ | LMF=811 and LMF=812 for a decimation ratio of 4 | ||
+ | LMF=421 and LMF=422 for a decimation ratio of 16 | ||
+ | LMF=821 and LMF=822 for a decimation ratio of 8 | ||
+ | LMF=442 and LMF=444 for a decimation ratio of 30 | ||
+ | LMF=841 and LMF=842 for decimation ratios of 15 and 16 | ||
- | |||
====== Typical Setup ====== | ====== Typical Setup ====== | ||
{{ : | {{ : |