Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:ad9208-3000ebz [28 May 2021 07:27]
Mark Arthur Recio
resources:eval:ad9208-3000ebz [12 Jul 2021 11:42]
Mark Arthur Recio added provision for Fsx4 mode for ad9699/ad9208
Line 112: Line 112:
   - The AD9208/​AD9689 plug-in should appear as in Figure 8 if installed properly. <​WRAP><​note>​Note:​ The AD9699 evaluation board shares the same plugin with AD9208</​note></​WRAP>​   - The AD9208/​AD9689 plug-in should appear as in Figure 8 if installed properly. <​WRAP><​note>​Note:​ The AD9699 evaluation board shares the same plugin with AD9208</​note></​WRAP>​
   - If the AD9208/​AD9689 plug-in does not appear, or no board is detected, make sure the ADS7-V2 is powered on and the evaluation board is properly connected. Make sure that ACE has been updated to the most recent version and the necessary plug-ins have been installed.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​1.png?​direct&​200 |}}{{ :​resources:​eval:​ace_ad9689-2600_start.png?​direct&​200 |}}</​WRAP><​WRAP centeralign>//​Figure 8. ACE's AD9208 / AD9689 Plug-in//</​WRAP><​WRAP><​note>​Note:​ Differences may occur between ACE plug-in versions, including the version number seen in Figure 8 above or components in any of the other images below - however, these will not affect the performance of the part nor the fundamental features described in this user guide.</​note></​WRAP>​   - If the AD9208/​AD9689 plug-in does not appear, or no board is detected, make sure the ADS7-V2 is powered on and the evaluation board is properly connected. Make sure that ACE has been updated to the most recent version and the necessary plug-ins have been installed.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​1.png?​direct&​200 |}}{{ :​resources:​eval:​ace_ad9689-2600_start.png?​direct&​200 |}}</​WRAP><​WRAP centeralign>//​Figure 8. ACE's AD9208 / AD9689 Plug-in//</​WRAP><​WRAP><​note>​Note:​ Differences may occur between ACE plug-in versions, including the version number seen in Figure 8 above or components in any of the other images below - however, these will not affect the performance of the part nor the fundamental features described in this user guide.</​note></​WRAP>​
-  - Click on the plug-in to open it. This will open the AD9208/​AD9689 Board View. Click the "​**Program FPGA Image**"​ button to program the ADS7-V2'​s FPGA for communicating with the AD9208-3000EBZ/​AD9689-2600EBZ. Once it is done programming,​ double click on the blue AD9208 / AD9689 chip (in the middle of the board) to open up the Chip View.<​WRAP><​note warning>​**Warning:​ Programming the FPGA will power the AD9208 evaluation board via the FMC connector. Removing any of the board'​s power jumpers (as seen in Figure 6) while the board is on or in operation may cause damage to the board, board components, and/or the chip. Removing the board while it is being powered via the FMC connector may also cause damage to the board.**</​note></​WRAP><​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​a1.png?​direct&​300 |}}{{ :​resources:​eval:​ace_ad9689-2600_board_view.png?​direct&​200 |}}</​WRAP><​WRAP centeralign>//​Figure 9. ACE's AD9208 / AD9689 Board View// \\ //<fc #​ff00ff>​Note:​ The plugin might display some warnings/​errors. These can be ignored for now</​fc>//</​WRAP>​ <​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​2.png?​direct&​500 |}}</​WRAP><​WRAP centeralign>//​Figure 10. AD9208 Chip View// \\ //<fc #​ff00ff>​The AD9689 Chip view is similar to the AD9208 chip view</​fc>//</​WRAP>​+  - Click on the plug-in to open it. This will open the AD9208/​AD9689 Board View. Click the "​**Program FPGA Image**"​ button to program the ADS7-V2'​s FPGA for communicating with the AD9208-3000EBZ/​AD9689-2600EBZ. Once it is done programming,​ double click on the blue AD9208 / AD9689 chip (in the middle of the board) to open up the Chip View.<​WRAP><​note warning>​**Warning:​ Programming the FPGA will power the AD9208 evaluation board via the FMC connector. Removing any of the board'​s power jumpers (as seen in Figure 6) while the board is on or in operation may cause damage to the board, board components, and/or the chip. Removing the board while it is being powered via the FMC connector may also cause damage to the board.**</​note></​WRAP><​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​a1.png?​direct&​300 |}}{{ :​resources:​eval:​ace_ad9689-2600_board_view.png?​direct&​200 |}}</​WRAP><​WRAP centeralign>//​Figure 9. ACE's AD9208 / AD9689 Board View// \\ //<fc #​ff00ff>​Note:​ The plugin might display some warnings/​errors. These can be ignored for now</​fc>//</​WRAP>​ <​WRAP>​{{ :​resources:​eval:​fig_10.jpg?​direct&​600 |}}</​WRAP><​WRAP centeralign>//​Figure 10. AD9208 Chip View// \\ //<fc #​ff00ff>​The AD9689 Chip view is similar to the AD9208 chip view</​fc>//</​WRAP>​
  
 ==== Obtaining a Full Bandwidth Capture ==== ==== Obtaining a Full Bandwidth Capture ====
-  - Under Initial Configuration,​ change the number of Virtual Converters to 1. Click Apply to apply the chip settings. Set the reference clock to the appropriate frequency as recommended by the ACE plugin.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​3.png?​direct&​400 |}}{{ :​resources:​eval:​ace_ad9689-2600_summary.png?​direct&​400 |}}</​WRAP><​WRAP centeralign>//​Figure 11. Chip Settings, AD9208-3000 on top, AD9689-2600 on bottom//</​WRAP><​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​4.png?​direct&​200 |}}</​WRAP><​WRAP centeralign>//​Figure 12. Apply Settings//</​WRAP>​+  - Under Initial Configuration,​ change the number of Virtual Converters to 1. Click Apply to apply the chip settings. Set the reference clock to the appropriate frequency as recommended by the ACE plugin.<​WRAP>​{{ :​resources:​eval:​fig_12.jpg?​direct&​400 |}}{{ :​resources:​eval:​ace_ad9689-2600_summary.png?​direct&​400 |}}</​WRAP><​WRAP centeralign>//​Figure 11. Chip Settings, AD9208-3000 on top, AD9689-2600 on bottom//</​WRAP><​WRAP>​{{ :​resources:​eval:​figure_12.jpg?​direct&​400 |}}</​WRAP><​WRAP centeralign>//​Figure 12. Apply Settings//</​WRAP>​
   - The chip view will update to reflect the changes made to the board. If any changes are made, the chip can be read by clicking the Read All button.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​5.png?​direct&​100 |}}</​WRAP><​WRAP centeralign>//​Figure 13. Read All//</​WRAP>​   - The chip view will update to reflect the changes made to the board. If any changes are made, the chip can be read by clicking the Read All button.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​5.png?​direct&​100 |}}</​WRAP><​WRAP centeralign>//​Figure 13. Read All//</​WRAP>​
   - Issue a data path reset to the AD9208 by clicking its checkbox and clicking Apply Changes. The data path reset bit will automatically self clear.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​6.png?​direct&​250 |}}</​WRAP><​WRAP centeralign>//​Figure 14. Data path reset//</​WRAP><​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​7.png?​direct&​100 |}}</​WRAP><​WRAP centeralign>//​Figure 15. Apply Changes//</​WRAP>​   - Issue a data path reset to the AD9208 by clicking its checkbox and clicking Apply Changes. The data path reset bit will automatically self clear.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​6.png?​direct&​250 |}}</​WRAP><​WRAP centeralign>//​Figure 14. Data path reset//</​WRAP><​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​7.png?​direct&​100 |}}</​WRAP><​WRAP centeralign>//​Figure 15. Apply Changes//</​WRAP>​
Line 128: Line 128:
 The procedure to obtain a FFT using DDC is the same between AD9208 and AD9689. The steps below use the AD9208 as the example, but the same can be done to the AD9689 plugin with the sample rate set to 2.6GSPS. The procedure to obtain a FFT using DDC is the same between AD9208 and AD9689. The steps below use the AD9208 as the example, but the same can be done to the AD9689 plugin with the sample rate set to 2.6GSPS.
   - This section explains the steps needed to setup the AD9208-3000EBZ in a DDC (Decimal Down Converter) setup as shown in Figure 24. <​WRAP>​{{ :​resources:​eval:​lmfs_4421_generic.png?​direct |}}</​WRAP><​WRAP centeralign>//​Figure 24. AD9208 DDC setup block diagram//</​WRAP>​   - This section explains the steps needed to setup the AD9208-3000EBZ in a DDC (Decimal Down Converter) setup as shown in Figure 24. <​WRAP>​{{ :​resources:​eval:​lmfs_4421_generic.png?​direct |}}</​WRAP><​WRAP centeralign>//​Figure 24. AD9208 DDC setup block diagram//</​WRAP>​
-  - Under Initial Configuration,​ set the Chip Operating Mode for two DDCs. **For AD9699, set the DDC inputs to Channel A only.** The DDC settings will become available, and automatically set up for Decimate-by-4 mode. For the decimation, select "​HB1_HB2_HB3 Complex"​ - three half-band filters, i.e. Decimate-by-8. Set the number of lanes to 4, the number of converters to 4, and the number of Octets per Frame to 2. Apply the settings. <​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​16.png?​direct&​400 |}}</​WRAP><​WRAP centeralign>//​Figure 25. DDC Chip Settings//</​WRAP>​+  - Under Initial Configuration,​ set the Chip Operating Mode for two DDCs. **For AD9699, set the DDC inputs to Channel A only.** The DDC settings will become available, and automatically set up for Decimate-by-4 mode. For the decimation, select "​HB1_HB2_HB3 Complex"​ - three half-band filters, i.e. Decimate-by-8. Set the number of lanes to 4, the number of converters to 4, and the number of Octets per Frame to 2. Apply the settings. <​WRAP>​{{ :​resources:​eval:​fig_25.jpg?​direct&​600 |}}</​WRAP><​WRAP centeralign>//​Figure 25. DDC Chip Settings//</​WRAP>​
   - The chip view will update to reflect the changes. Click on the NCO block to change the Numerically Controlled Oscillator'​s frequency to 1300 MHz. Enable the 6dB gain for the DDC from the dropdown menu. Click Apply Changes to apply both.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​17.png?​direct&​200 |}}</​WRAP><​WRAP centeralign>//​Figure 26. NCO Frequency Setting//</​WRAP><​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​18.png?​direct&​200 |}}</​WRAP><​WRAP centeralign>//​Figure 27. DDC Gain//</​WRAP>​   - The chip view will update to reflect the changes. Click on the NCO block to change the Numerically Controlled Oscillator'​s frequency to 1300 MHz. Enable the 6dB gain for the DDC from the dropdown menu. Click Apply Changes to apply both.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​17.png?​direct&​200 |}}</​WRAP><​WRAP centeralign>//​Figure 26. NCO Frequency Setting//</​WRAP><​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​18.png?​direct&​200 |}}</​WRAP><​WRAP centeralign>//​Figure 27. DDC Gain//</​WRAP>​
   - Navigate to the second DDC (DDC1) and make the same changes.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​19.png?​direct&​200 |}}</​WRAP><​WRAP centeralign>//​Figure 28. DDC Selection//</​WRAP>​   - Navigate to the second DDC (DDC1) and make the same changes.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​19.png?​direct&​200 |}}</​WRAP><​WRAP centeralign>//​Figure 28. DDC Selection//</​WRAP>​
   - In Analysis, run a capture. DDC0 can be selected from Channel A and DDC1 can be selected from Channel B.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​23.png?​direct&​200 |}}</​WRAP><​WRAP centeralign>//​Figure 29. DDC Selection//</​WRAP>​   - In Analysis, run a capture. DDC0 can be selected from Channel A and DDC1 can be selected from Channel B.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​23.png?​direct&​200 |}}</​WRAP><​WRAP centeralign>//​Figure 29. DDC Selection//</​WRAP>​
   - A successful capture is shown below, with a filtered 1305 MHz signal input to Channel A / DDC0.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​22.png?​direct&​600 |}}</​WRAP><​WRAP centeralign>//​Figure 30. AD9208-3000 DDC FFT at 1305MHz Analog Input to Channel A; NCO tuning frequency = 1300MHz//</​WRAP> ​   - A successful capture is shown below, with a filtered 1305 MHz signal input to Channel A / DDC0.<​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​22.png?​direct&​600 |}}</​WRAP><​WRAP centeralign>//​Figure 30. AD9208-3000 DDC FFT at 1305MHz Analog Input to Channel A; NCO tuning frequency = 1300MHz//</​WRAP> ​
 +
 +==== Setting up AD9208/​AD9699 Fsx4 Mode ====
 +Fsx4 mode on AD9208/​AD9699 is only supported using [[adi>​en/​content/​CU_High-Speed_ADC_FIFO_evaluation_tools/​fca.html#​ADS8-V1|ADS8-V1]]. The procedure below shows how to use Fsx4 mode with ADC sampling frequency of 3GHz and a Reference clock of 600MHz.
 +  - On the Chip Application Mode tab, click on the Fsx4 Operation dropdown menu and select "L/M = 4/1" for AD9699, "L/M = 8/2" for AD9208. <​WRAP>​{{ :​resources:​eval:​fsx4_mode.jpg?​direct&​600 |}}</​WRAP><​WRAP centeralign>//​Figure 31. AD9699 Fsx4 mode setting//</​WRAP> ​
 +  - Source the required REFCLK to the [[adi>​en/​content/​CU_High-Speed_ADC_FIFO_evaluation_tools/​fca.html#​ADS8-V1|ADS8-V1]].
 +  - Click Proceed to Analysis. This is ACE's Analysis tool for data from the ADC, displaying both sample plots and FFTs. Click on FFT and run one capture.
 +  -  A successful capture is shown below, with a filtered 255 MHz signal input to Channel A. <​WRAP>​{{ :​resources:​eval:​user-guides:​ad9208:​stepbystep:​15.png?​direct&​500 |}}</​WRAP><​WRAP centeralign>//​Figure 32. AD9208-3000 Fsx4 FFT at 255MHz Analog Input to Channel A//</​WRAP>​
  
 ====== Troubleshooting Tips ====== ====== Troubleshooting Tips ======
resources/eval/ad9208-3000ebz.txt · Last modified: 12 Jul 2021 11:42 by Mark Arthur Recio